Set a line trigger

Prev Next

Internal line trigger

The internal line trigger provides a continuous signal in the frequency of the Acquisition Line Rate.

  1. In the Configuration window navigate to Acquisition Control → Line Trigger.
  2. Below Internal select the Generate line trigger at frequency of line rate checkbox.

Ein Bild, das Text enthält.  Automatisch generierte Beschreibung

Alternatively, you can set the internal line trigger in the camera feature tree by executing the following step:

StepFeature nameValue
1Trigger SelectorLineStart
Trigger ModeOff

External line trigger

The external line trigger can be provided by an encoder signal or a signal generator. Refer to trigger selector.

  1. In the Configuration window navigate to Acquisition Control → Line Trigger.
  2. Below External select the Generate line trigger from external encoder signal checkbox.
  1. In Encoder Source A and B select the desired input Line. Refer to electrical installation. 
  2. In Line Format select the electrical input signal. Refer to electrical installation.
  3. In Encoder Divider float input the number of encoder impulses to generate one LineStart signal. Refer to Encoder divider float.
  4. In Encoder Average input the number of averaged input signals.


Alternatively, you can set the external  line trigger in the camera feature tree by executing the following steps:

StepFeature nameValue
1TriggerSelectorLineStart
TriggerModeOn
2TriggerSourceEncoder0
or Line1
or Line3
or Line4
3EncoderSelectorEncoder0
4EncoderSource ALine1
5EncoderSource BLine2
6EncoderDividerFloat0.05 – 255
7EncoderAverage0-16
8Digital I/O Line Selector select the Trigger Source 
9Line Formatopen the drop-down menu and change the Line Format to your input signal


Trigger Source 

Encoder0

The Trigger Source  Encoder0 triggers the LineStart of the image acquisition. A certain number of encoder (Encoder divider float) impulses creates one LineStart signal. 

svg-signal diagram-encoder 2 channel_03


Line 

The Trigger Source  Line triggers the LineStart of the image acquisition. Each impulse generates one LineStart signal. 

svg-signal diagram-wave_03


Encoder divider float 

An encoder typically does not have an integer ratio to the camera resolution. Arbitrary ratios of encoder pulses per sensor line are possible, for example, 2.25. The value range is 0.05 – 255 pulses per line.

Example:

  • Linear Stage with a tread pitch of 1 mm
  • Encoder with a resolution of 1000 Impulses per turnaround (I/U) → 1 Impuls per µm 
  • Optical lateral Camera resolution of 10 µm 

Encoder divider float =  Optical resolution x encoder transport resolution = 10 µm x 1 I/µm = 10 I            Missing argument for \widehat   \widehat          Missing argument for \widehat  \widehat