Electrical installation

Prev Next

DXGE interface

The SFP+ 10 GigE connectors permit to use (direct attach) copper cables or optical fiber cables with lengths of up to 400 m (10GBASE-SR).

  • Use a single port for data rates up to 10 Gbit/s.
  • For higher data rates connect both ports using Link Aggregation.

Network adapter

To establish a DXGE connection a network adapter with one or two SFP+ 10 GigE inputs must be installed and configured on the PC. The installation of a network adapter is explained in the GCT documentation. For more information, see Installation GigE. 

For more information about the tested network adapters and the transceivers, see Tested Network adapters and Transceivers.

Cabling

electricitygeneral warningWARNING
Electric shock due to improper connection to a power supply.
Use a 12 V – 24 V DC power supply.
  1. Connect one or both video output ports.
  2. Connect the digital I/O port.
  3. Connect the power supply.

CXP interface

The interface allows you to connect up to four CXP cables. Micro BNC (for CXP12) connectors for the camera and suitable connectors for the frame grabber are required. The maximum cable length is 35 m.

Frame grabber

To establish a CXP connection a frame grabber must be installed and configured on the PC. Refer to the manual of your frame grabber. 

For more information about the tested frame grabbers, see Tested frame grabbers.

Cabling

electricitygeneral warningWARNING
Electric shock due to improper connection to a power supply.
Use a 12 V – 24 V DC power supply.
  1. Connect port 0 (master port) of the video output port.
    NOTE
    For the maximum line rate connect all four ports.
    Make sure that port 0 of the camera is connected to port 0 (or A) of the frame grabber. Otherwise, no connection to the camera can be established.
  2. Connect the digital I/O port.

Option 1: Power over CoaXPress (PoC)

To use the power-over-CXP function two connections are needed.

Connect port 0 and port 1 of the video output port.

Option 2: Power supply port

Connect the power supply.

Digital I/O port

NOTE
Ensure a proper GND connection of the digital camera I/O port and your trigger.  

The following connector is required for the digital I/O port:

  • 15-pin HD D-Sub (male)

evo-digital io_02Pin allocation D-Sub connector (female) of the camera

PinGenICamSignalLevelIn/OutExample/Remark
1Line 1
Enc0_InP (+)
RS 422
Differential input
Encoder0 or LineTrigger
2Line 2
Enc1_InP (+)
RS 422
Differential inputEncoder1 or Frametrigger
3Line 3
IO_0P
LVCMOS
Input
single-ended
4-RT
RS 485
--
5Line 5
IO_2P
LVCMOS
OutLED-Out1
6Line 1
Enc0_InN (-)
RS 422
Differential input
Encoder0
7Line 2
Enc1_InN (-)
RS 422
Differential input
Encoder1
8Line 4
IO_1N
LVCMOS
Input single-ended
Trigger or Master-Slave Cascaded
9-RTN
RS 485
Out
To LightController XLC4
10Line 6
IO_3
LVCMOS
Out
LED-Out2
11-GND
-GND-
12Line 7
IO_4_SDA
LVCMOS
Out
LED-Out3
13-GND
GND
--
14Line 9Master/Slave
LVCMOS
Bi-directional
Master/Slave
15Line 8
IO_5_SCL
LVCMOS
Out
LED-Out4

LVCMOS and RS422 levels

I/O standardV_ILV_IHV_OLV_OH

V_minV_maxV_minV_maxV_maxV_min
LVCMOS–0.50.71.73.60.42.1
RS422–60.826--
noticeNOTICE
Non compliance may cause irreparable damages to the device.
The maximum input level of the LVCMOS is 3.6 V.
Use a level converter if necessary (e.g. 74 LVC14).


Circuit Diagrams

RS422 configuration

svg-neo-circuit_diagram_rs422External circuit:  RS422 device

Single-Ended configuration

svg-neo-circuit_diagram_1External circuit: Optocoupler

svg-neo-circuit_diagram_2External circuit: TTL or CMOS logic gate  

Power supply

The following connector is required for the power supply cable:

  • Manufacturer: Hirose
  • Article no.: HR10A-7P-6S female

PinDescription
svg-evo-power supplyPin allocation of the power supply port

 

1Power +24 V
2Power +24 V
3Not connected
4Not connected
5Ground
6Ground