Network adapters and transceivers

Prev Next

SFP+ connection

Note

If you are using the s2i Transport Layer it is required to configure the network adapter properly. The HPE Ethernet 10Gb 2-port 560SFP+ Adapter and Intel (X710) are configured during installation. 

* Some manufacturers encode their cards. Those cards can only be used with the appropriate transceivers.
Example: Intel X710 chipsets only work with Intel or Intel-configured transceivers

Network adapter

The following network adapters are tested with GCT2. The results are shown in the following table.

Vendor Name

Type

Result

S2i TL

Kithara TL

HPE

HPE Ethernet 10Gb 2-port 560SFP+ Adapter

Fully functional

X

X

HPE *

HPE Ethernet 10Gb 2-port 562SFP+ Adapter

Not supported yet



Intel *

Intel® Ethernet-Converged-Network-Adapter X710

Fully functional

X

X

Myricom

Myricom 2x 10GbE SFP+ low-profile NIC

Only with s2i

X


Myricom

Myricom 1x 10GbE SFP+ low-profile NIC

Only with s2i

X


Mellanox

NVIDIA Mellanox MCX512A-ACAT ConnectX®-5 EN Network adapter

Only with s2i

X


Broadcom

P210P - 2 x 10GbE PCIe NIC

Only with s2i

x

Zebra

GevIQ 

Fully functional 

Zebra TL

Installation 

Network adapter 


HPE Ethernet 10Gb 2-port 560SFP+ Adapter

Download and install the following files

Download the Wired_dirver_xx and the Wired_PROSet_xx from the Intel Homepage.

Network adapter with X550 Intel chipset

Download and install the following files

Download the Wired_dirver_xx and the Wired_PROSet_xx from the Intel Homepage.

Network adapter with X710 Intel chipset

Download and install the following files

Download the Release_xx from the Intel Homepage.

Broadcom P210P

Download an install the following files

Download the Release_xx from the Broadcom Homepage

Zebra GevIQ 

Download and install the following files

Download the Release_xx from the Zebra Homepage.


Transceiver

The following transceivers are tested with the allPIXA evo camera and the network adapters.

Vendor Name

Type

Comment

Camera side

Network adapter side

Finisar

FTLX8574D3BCL

Class 1 21CFR1040:10


X

X

FS

SFP-10GSR-85


X

X

FS

Intel E10GSFPSRX Compatible 10GBASE-SR SFP+ 850nm 300m DOM Duplex LC MMF Transceiver Module

Recommended for Network adapters that are marked with *


X


RJ45 connection 

Network adapter 

The following network adapters are tested with GCT2. The results are shown in the following table.

Vendor name

Type

Result 

s2i TL 

Kithara TL 

Broadcom

P210TP - 2 x 10GBASE-T PCIe NIC

Fully functional 

X


Installation 

1. Download the driver file and follow the installation instructions.

Download

For the Broadcom Network adapter "P210TP - 2 x 10GBASE-T PCIe NIC", you can find the download files here.