Performance Test

Prev Next

The GCT installer provides a performance test tool. The tool allowed you to analyze the performance of your camera connection.

Performance Test tool folder 

C:\Users\Public\Documents\Chromasens\GCT2\performanceTest

On your desktop, you can find a direct link to the performance test, therefore double-click the desktop link "Testperformance GCT2".
The folder provides three different .bat files. These files are predefined examples to run the performance test. 

Name 

Description

performanceTestCompatHelp.bat


Opens the Help dialog of the performance test tool 

runPerformanceTestCSIGeneric.bat


Opens a generic configuration of the performance test tool, which can be used for CXP and Gige Cameras 

runPerformanceTestCSIwithKithara.bat


Opens the performance test tool for Kithara configured cameras 

runPerformanceTestCSIwiths2i.bat

Opens the performance test tool for S2I configured cameras 



Parameter description 

The program has the following adjustable parameters:

Parameter 

Entries 

Description

--checkImageConsistency 


 GreyHorizontalRamp or GreyHorizontalRampMoving

Method for checking error proune images

--checkImageConsistencyOption

MTSTD (STSISDComplete or STSISD)

Option for checking error proune images

--deviceSelection  

auto or manual

"auto" selects the first visible device, "manual" you can select the device 

--height  


Height in pixel

--help


Performance tool options

--line_time_step_width


Number of microseconds to increase from one test run to the next

--pixelFormat  

RGB8, Mono8....

GeniCam SFNC Pixel Format

--reportFileDir


Option for setting directory of the written report file

--ring_buffer_count 


Number of used frame buffers

--single_test_duration


Duration in seconds for a single integration time

--start_line_time  


Line time to start with in us.

--stop_line_time


When this line time is reached, the test will be stopped.

--use_filter_driver

1 and 0 

1 for on or 0 for off, default off

--width 


Width in pixel

Example of a command line:

PerformanceTest.exe --use_filter_driver 1 --single_test_duration 3 --start_line_time 60 --line_time_step_width 3 --stop_line_time 65 --pixelFormat RGB8 --checkImageConsistency GreyHorizontalRamp

This means the camera uses RGB8 as image format, starts with an acquisition line time of 60 microseconds (us), stops after 65 us, and the step is 3 us. With each acquisition line time, the test of each different line time will take 3 seconds. The filter driver for the S2I transportlayer is set to "on".  An image consistency check is done with the "GreyHorizontalRamp". The running program can be stopped by pressing any key.


Results and Output

The output of the Performance Test Tool is shown in the command line window and in the Test Reports folder. 

Test Reports Folder 
C:\Users\Public\Documents\Chromasens\GCT2\performanceTest\TestReports

Parameter 

Description 

Duration [s]

Acquiring time in seconds 

Line/Frame Time [us]

Set line time in microseconds 

Acquired 

Acquired frames 

Dropped 

Dropped frames 

Corrupted (N/Min/Max)

Number of corrupted pixels N = corrupted images, Min = Minimum number of corrupted pixels in one image, Max = Maximum number of corrupted pixels in one image 

Packets OK 

Number of transmitted packets without an error

Packets Error 

Number of transmitted packets with an error

First Frame Packets Error 

Packet error in the first frame 

GBit/s

Transmission rate 

*(-1 means that this method was not used for this test)