Documentation Index

Fetch the complete documentation index at: https://docs-linescan.alliedvision.com/llms.txt

Use this file to discover all available pages before exploring further.

User level

Prev Next

Each camera contains an XML file specifying the available camera features. When GCT connects to the camera, it loads the XML file and shows the features as a tree structure.

Each feature has a visibility level. While all features are displayed for user-level Developers, many advanced features are hidden for user-level Beginner.

The User Level is shown above the feature area. To modify the user level, click the displayed User Level, and then click the desired level:

Graphical user interface, text, application  Description automatically generated