Documentation Index

Fetch the complete documentation index at: https://docs-linescan.alliedvision.com/llms.txt

Use this file to discover all available pages before exploring further.

allPIXA neo

Prev Next

For all neo cameras, passive and active cooling kits are available, which can be mounted to the back, upper, or lower side of the camera

DescriptionIdentification Number 
allPIXA neo PIN Cooling CP000666
allPIXA neo FAN CoolingCP000667


Pin Coolingneo_pin_cooling

Fan Cooling 

Download as pdf-file