Documentation Index

Fetch the complete documentation index at: https://docs-linescan.alliedvision.com/llms.txt

Use this file to discover all available pages before exploring further.

allPIXA evo

Prev Next

For all evo cameras, passive and active cooling kits are available, which can be mounted to the back, upper, or lower side of the camera


A picture containing electronics, computer  Description automatically generatedallPIXA evo with PIN Cooling

 



DescriptionIdentification Number 
allPIXA evo PIN Cooling CP000643
allPIXA evo FAN CoolingCP000644
allPIXA evo Water CoolingCP000651


Pin Cooling 

evo_pin_cooling

Download as pdf-file

Fan Cooling 

Note
To start the fan you need to enable the Device Fan Enable flag, see the installation chapter. 

evo_fan_cooling

Download as pdf-file

Water Cooling

Note

For connecting the liquid heat sink we recommend a pipe 8 mm diameter inside and 10 mm outside diameter material PA-pipe.

For liquid, we recommend a water-glycol mixture with min-18% glycol to avoid algae in the liquid.

But check with the producer of the cooling system. Often, they need an additional additive to avoid corrosion in the system.

On tested cooling system is the following one: ⁣External cooling system AQ240-Pro - High Power | innovatek Webshop (webshop-innovatek.de)


evo_water_cooling

Download as pdf-file

Installation 

  1. Place heat-conducting pads between the camera and the cooling adapter. Different pads are included, choose the pad which fits best to the camera side. 
  2.  Mount the cooling adapter. 
  3.  For fan cooling, connect the power supply cable with the camera's fan power supply connector. 
  4.  For fan cooling, enable the fan in your camera. Open the camera in GCT and navigate to the camera feature tree and set the parameter Device Fan Enable to true and save the setting.