Overview

Prev Next

The cameras offer CMOS performance with CCD image quality. There are line rates possible of up to 300 kHz.

The cameras fulfill the GenICam standard communication protocol. You can set up the camera, browse and adjust parameters with every tool that fulfills the GenICam standard. The provided Allied Vision  GCT software is available for Windows and Linux.

svg-camera-software communication_03Scheme of the communication between a host and the camera 


Firmware and software version

This documentation refers to the following version:

Camera: Packet 1.1.0

Feature reference

For detailed information on camera controls refer to the feature reference. It describes the standard and advanced camera control. 

Make sure that you always refer to the feature reference that matches the used firmware version.

Software GCT

Refer to the GCT documentation for the following information: 

  • Installation and use

  • Configuration of the PC depending on the camera interface

EMVA Reports

The EMVA1288 report is not available on the online documentation.

For more information, please contact our support team.