NOTE: Finding camera and illumination parameter
This method of finding a starting point for a standard camera and illumination system. The operating point may have to be determined iteratively (requirement of the application).
At the beginning of the calibration process, the brightness of the camera output image must be in a reasonable range. Otherwise, the white balancing will most likely fail or the result quality will be poor. White balancing is an automatic camera gain adjustment algorithm. It sets the gains (amplification factors) for the single color channels in a way, that the brightness of the color channels equals the defined target brightness level for a given object. However, to achieve the best image quality these gains should be always kept as low as possible (In the best case between 1 and 2). To achieve a brightness level of 200DN@8bit with an amplification factor <2, the brightness of the single color channels must be >100DN@8bit for the default gain of 1. It should be mentioned again that a factor of less than 2 is preferable but not required and often not possible.
Camera Parameter
Before starting, set the following parameter.
NOTE
You can also load the “Default” user set.
| ![]() |
| ![]() |
| |
| |
| |
| ![]() |
|
Exposure time
NOTE
Always set the exposure time as high as possible. The exposure time is limited by the line time. There are 2 cases for the line time.
Case 1: Freerun | |
|---|---|
| ![]() |
| ![]() |
| ![]() |
Case 2: Line trigger mode | |
|---|---|
| |
| Transport speed / Optical resolution in transport direction |
| Measure the line time
![]() |
|
![]() If the Status is Speed to High your exposure time is too high |
Sensor Sensitivity
NOTE
“SensorSensitivity” is a GenIcam parameter to change the analog amplification and the full well capacity of the sensor. It is better to have a high sensor sensitivity than high gains since the amplification is earlier in the camera signal processing chain. Therefore, fewer sources of noise are amplified. However, a high sensor sensitivity nevertheless increases the noise of the resulting image.
| |
| ![]() |
Lens aperture
NOTE
Choosing the lens f-stop is always a compromise between the available amount of light and depth of field. Reducing the f-number by one step (e.g. from f/8 to f/5.6) doubles the amount of light of increases the DOF.
Allied Vision approch
This is a Allied Vision approch, it does not fit to all setups
Start as a starting point f = 5.6
If a higher depth of field is required set f = 8.0 (half amout of light)
Illumination
Alignment
NOTE
Always mount the illumination regarding the mechanical specifications. Especially for strongly focused illuminations (darkfield C and B focus), it is recommended to fine-tune the alignment.
It’s important to start with a well-aligned illumination to avoid wasting light.
| |
| ![]() |
| |
| |
| |
|
Current
NOTE
For the image quality in terms of image noise, it is beneficial to use a high illumination current. However, a high illumination current also has disadvantages caused by the high temperature of the light source.
Reduces the lifetime of the LEDs.
Can harm the scanned object.
Causes heat inducted turbulences which can locally distort the image which is disadvantageous for high precision measurement tasks.
Can lead to overheating of the illumination if it is not cooled actively.
| For a passive cooling, start with 600 mA For an active cooling, start with 1200 mA |
| |
| |
|
.png)
.png)
.png)
.png)
.png)
.png)
.png)
.png)
.png)