Safety

Prev Next

Safety instructions

  • Operate the device only in a faultless and safe condition.

  • Modifications and extensions to the device are only permitted if the prior written consent of Allied Vision  GmbH is obtained.

  • Comply with the ambient conditions described in this manual.

  • During operation do not touch the hot surface of the device.

  • During operation do not look into the light.

  • Do not remove warning signs form the device.

  • Keep away from liquids.

  • Use the original packaging for transportation.

Safety instructions on optical radiation

Intense light sources can have the following effects to the human body:

  • Temporary reduction in visual acuity

  • Visual impairment

  • Afterimages

  • Irritation

  • Annoyance

  • Leading to accidents

Follow the safety instructions:

  • Do not look into the light beam.

  • Check the device before every use.

  • Wear opaque eye protection.

Optical radiation risk classes

The LEDs in the Corona II are divided into risk classes according to the risk assessment system CIE S009/E:2002 (DIN EN 62471).

The classification is done at full power operation. At lower current rates, the risk class might be lower.

Dark field

LED

Reflector type

Top light A

Top light B

Top light C

Top light D

White

Class 2 “Medium risk”

Class 2 “Medium risk”

Class 1 “Low risk”

Class 1 “Low risk”

Red, green

Class 1 “Low risk”

Class 1 “Low risk”

Class 1 “Low risk”

Class 1 “Low risk”

Blue, IR

850 nm / 940 nm

Class 2 “Medium risk”

Class 2 “Medium risk”

Class 2 “Medium risk”

Class 2 “Medium risk”

UV

365 nm / 395 nm

Class 3 “High risk”

Class 3 “High risk”

Class 3 “High risk”

Class 3 “High risk”

SWIR

1100 nm / 1550 nm

Class 1 “Low risk”

Class 1 “Low risk”

Class 1 “Low risk”

Class 1 “Low risk”

Bright field

LED

Reflector type

Bright field H

White, red, green

Class 1 “Low risk”

Blue, IR

850 nm / 940 nm

Class 2 “Medium risk”

UV

365 nm / 395 nm

–

SWIR

1100 nm / 1550 nm

–

Tube light

LED

Reflector type

Tube light T, U

White, red, green

Class 1 “Low risk”

Blue, IR

850 nm / 940 nm

Class 2 “Medium risk”

UV

365 nm / 395 nm

–

SWIR

1100 nm / 1550 nm

–

Safety instructions on thermal risks

The operating temperature of the device might be 75 °C. Hot surfaces can cause skin burns.

Follow the safety instructions:

  • Install additionally housings or covers to prevent skin burns.

  • Always switch off the device before carrying out any work on it.

Meaning of the signal words, safety signs and graphical symbols

Signal words

The following signal words are used in this manual:

Signal wordMeaning, consequences if not prevented
DANGER

Warns of an imminent hazardous situation which results in death or serious injury.

WARNING

Warns of a potential hazardous situation, which could result in death or serious injury.

CAUTION

Warns of a potential hazardous situation, which could result in minor or moderate injury.

NOTICE

Warns of a hazardous situation, which can result in material damage or environmental damage.

Safety signs and graphical symbols

The following safety signs and graphical symbols are used:

Sign

Meaning

electricity

Warning of dangerous electrical voltage

hazard warning sign-optical radiation

Warning of optical radiation

hazard warning sign-flammable material

Warning of flammable material

falling items

Warning of falling items

hot surface

Warning of hot surface

notice

Warning of potential damage to the device

image-1674813282773

Indicates that electrical and electronic equipment should not be disposed with normal garbage at the end of its working life.

Personnel requirements

Untrained person

The untrained person has been instructed by the operating company or an authorised representative of the operating company (qualified personnel) about the tasks assigned to him and the possible dangers in case of improper behaviour. The untrained person has been instructed about the protective measures and the operating tasks. The untrained person has sufficient knowledge of the national language, both written and spoken.

Qualified personnel

Qualified personnel are persons who, due to their professional training, knowledge and experience as well as knowledge of the relevant standards and regulations, carry out the work assigned to them, assess it and independently recognize possible dangers independently. The person knows the operating instructions of the machine. Skilled personnel are mechanics, electricians and technicians.

Assignment of the tasks

Task

Untrained person

Qualified personnel

Installation

Prohibited

Allowed

Programming

Prohibited

Allowed

Calibration

Prohibited

Allowed

Testing

Prohibited

Allowed

Cleaning

Allowed

Allowed

Repairing

Prohibited

Prohibited