Maintenance and disposal

Prev Next

Safety instructions

  • Only technicians of Allied Vision  GmbH are permitted to open or slacken screws or housing sections of the device.

  • Before carrying out any work on the device disconnect the power supply.

  • To avoid the risk of fire let other devices such as radiators, heaters or lightning equipment cool down first.

  • Necessary repairs may only be carried out by Allied Vision  GmbH.

hot surfacegeneral warningCAUTION
The device can heat up to 60 °C.
Do not touch the hot surface.
Let the device cool down before carrying out any work on it.

Cleaning

During operation of the device, particles such as dust etc. may be settled on the lens. These deposits affect the quality of the optical image and the function of the device negatively.

Cleaning intervals

Specify regular cleaning intervals depending on your ambient conditions and the degree of soiling.

Cleaning procedure

  1. Disconnect the power supply.

  2. Let the device cool down. Wait at least 30 minutes.

  3. Wipe all surfaces with a soft and lint-free cloth, starting with the lens. The use of isopropanol ist optional, refer to the manufacturer's manual.

  4. Inspect the device to ensure that cleaning was effective and repeat if necessary.

Repair

In case of damages to the device refer to Allied Vision  GmbH.

Disposal

image-1674813282773

This product is an electronic device.
Please dispose this product in accordance with your local regulations. Contact your local government office for details about environmentally safe recycling.