Documentation Index

Fetch the complete documentation index at: https://docs-linescan.alliedvision.com/llms.txt

Use this file to discover all available pages before exploring further.

FAQ

Prev Next

FAQ

What is the maximum line rate of the allPIXA neo 4k GigE

The maximum line rate for the camera is

Configuration Line rate
Mono (8 bit) 249.7 kHz
RGB (8 bit) 88.4 kHz
RGB + Mono (8 bit) (NIR)69.9 kHz

I can’t increase the line rate of the camera, what could be the reason?

The exposure time can limit the maximum line rate, the exposure time must be shorter than the line time. Try to reduce the exposure time.

The bandwidth of the connection can also limit the maximum line rate. Make sure that the 10 GigE connection is stable.

I can't get a connection to the camera what could be the reason?

Please take a look at the following article, which describes how the problem can be solved.

Troubleshooting with GigE Interface