The GCC.ini file, which is located under C:\Users\Public\Documents\Allied Vision\GCT2, including the content of producer path, producer filename, and selected producer for the discovery are already adjusted automatically in the file GCC.ini. file. Therefore, if the discovery has already been executed, the file GCC.ini could look as follows in the block of [DefaultProducers].

- ProducerList contains the found cti transport layer files.
- AdditionalSearchPath contains the additional search paths for cti files, which can be added by clicking Add Producer Path.
- SelectedProducerList contains the cti transport layer files which are selected to be applied for the discovery process.