Documentation Index

Fetch the complete documentation index at: https://docs-linescan.alliedvision.com/llms.txt

Use this file to discover all available pages before exploring further.

Create a black-reference (DSNU)

Prev Next

Create a black-reference with DSNU.

  1. Switch off the illumination.

  2. Cover the lens with a black or dark piece of cardboard or plastic.
    No light may reach the sensor.


  1. In the menu bar navigate to ToolsCalibration.

  2. Click Generate DSNU Reference.



The Generate DSNU Reference wizard opens.

  1. Click Acquire image to generate the DSNU directly from the camera
    or
    click Load from Disk to load an image from the hard drive.

    NOTE: Load from Disk

    Make sure that the image has been taken with active image calibration mode by using the wizard.

The raw image and the line plot of the image is displayed. 

Send the calculated DSNU to the camera: 

  1. Select LUT 1 or LUT 2.

  2. Click Send data to camera.



  1. In the Configuration window navigate to Camera Image CalibrationDSNU/PRNU.

  2. Make sure that DSNU is enabled.


getting-started-image-20n4f0fx