Acquire images with frame and line trigger

Prev Next

Set up the frame trigger

  1. In the Configuration window navigate to Acquisition Control → Frame Trigger.
  2. Set up the frame trigger.  
Refer to Set a frame trigger.



frame_trigger_singel_ended

Set up the line trigger

  1. In the Configuration window navigate to Acquisition Control → Line Trigger.
  2. Set up the line trigger.
  3. Acquire an image.
Check your cabling if you do not receive an image.
Refer to Set a line trigger. 

linetrigger_encoder(1)