If an error is set, an error response is generated.
Examples
Query | Response | Meaning |
|---|---|---|
MU 1 | er 100 | unknown command |
IY K 500 | er 101 | unknown parameter |
IY A 4000 | er 102 | parameter out of range |
If an internal error is set, the response is integrated in the standard response: | ||
TE | te 70-80,71,23-21,22;er 202,A | LED voltage at channel A out of range |
List of error codes
Error code number | Description |
|---|---|
100 | Unknown command |
101 | Unknown parameter |
102 | Parameter out of range |
103 | Command is not allowed in the current operating mode |
200 | Supply voltage exceeds limits |
201 | Analog control voltage exceeds limits |
202 | LED Voltage out of range |
203 | Output voltage exceeds limits (Programmed in the Corona II module) |
204 | Warning temperature exceeded |
205 | Maximum temperature exceeded |
206 | Shutdown active |
210 | Write error to EEPROM in Driver Unit |
211 | Read error from EEPROM in Driver Unit |
212 | Write error to EEPROM in Corona |
213 | Read error from EEPROM in Corona |
214 | Fan failure detected at ACTRL |
215 | Programmable voltage value out of range (Programmed in the XLC4 control unit) |