Read each line info block

Prev Next

Decoding of the each line info block - RGB

Pixel

0

1

2

3

4

5

6

7

8

9

Red

Marker

Error code

Speed2high

Encoder clocks

Next line position

Time stamp

Unsupported

Unsupported

Unsupported

Marker

Green

Continuous line count

Line count

Line time

Blue

Continuous line count

This counter increments by 1 for each row of the image. The counter continues counting for new images and is not reset. It can be used to detect missing image information.

Structure


Continuous line count

–

Byte 1

Byte 0

Px0Red

Px0Green

Px0Blue

Decoding

The decoding of the continuous line count is:

Clc = Px0Green × 256 + Px0Blue

Example

Clc = 217 × 256 + 127 = 55679

svg-read each line-continuous line count_03

Example: Decoding of continuous line count 

Line count

This counter increments by 1 for each row of the image. The counter starts counting at 0 for each image. It can be used to detect missing image information.

Structure


Line count

–

Byte 1

Byte 0

Px1Red

Px1Green

Px1Blue

Decoding

The decoding of the line count is

Lc = Px1Green × 256 + Px1Blue

Example

Lc = 0 × 256 + 0 = 0

svg-read each line-line count_03

Example: Decoding of line count

Speed too high

This information can be used to check if the speed of the line trigger signal is too high for the camera. In this case, the camera switches to freerun and acquires with the maximum possible speed. This state must be avoided because the transport resolution of the image is not constant. If the flag is “True” for some lines there are the following options to avoid this issue.

The speed too high state can be caused by two parameters

  • Exposure time (Exposure time ≥ Line time - 2us offset)
    Compare the exposure time with the info block information “line time“ to check if the exposure time is the limiting factor.

  • Interface speed

To avoid the speed too high state there are multiple options.

  • Reduce the transport speed if possible.

  • If the info block information “line time“ oscillates heavily check the electrical connection or try to stabilize the mechanical transportation process.  

  • If the exposure time is the limiting factor reduce the exposure time.

  • If the interface speed is the limiting factor, increase the interface speed is possible (Use more CXP lanes or a faster CXP type / Use dual 10GigE)

Structure

Speed2high

–

Bit 7

Bit 6 – Bit 0

Px2Red

Line time

This information represents the line time. For an operation without a line trigger, this variable is constant and equal to the camera parameter line time. If the camera is triggered with a line trigger this information can be used to check the signal/mechanical transport quality.

  • If the signal oscillates very heavily with a high frequency the electrical connection is not OK.

  • Small oscillations (for example +-20%) are most probably mechanical vibrations in the transport process.
    These effects are typical for:

    • Belt drives

    • Conveyor belts

    • Low-quality linear stages for scans with a high resolution.

Structure


Line time clocks

Bit 7 – Bit 4

Bit 3 – Bit 0

Byte 1

Byte 0

Px2Red

Px2Green

Px2Blue

Decoding

The decoding of the line time is:

Lt = (Px2Red × 216 + Px2Green × 28 + Px2Blue) / 100

Example

Lt = (0 × 216 + 21 × 28 + 124) / 100 = 55 µs

svg-read each line-line time_03

Encoder clocks

Structure

Encoder clocks

Byte 2

Byte 1

Byte 0

Px3Red

Px3Green

Px3Blue

Decoding

The decoding of the encoder clocks is:

Ec = Px3Red × 216 + Px3Green × 28 + Px3Blue

Next line trigger position

Structure

Next lt pos raw

Byte 2

Byte 1

Byte 0

Px4Red

Px4Green

Px4Blue

Decoding

The decoding of the encoder clocks is:

Nlp = (Px4Red × 216 + Px4Green × 28 + Px4Blue) / 256

Time stamp

Structure

Time [s]

Time [¼ ms]

Byte 2

Byte 1

Byte 0

Px5Red

Px5Green

Px5Blue

Decoding

The decoding of the time stamp is:

Ts = (Px5Red × 216 + Px5Green × 28 + Px5Blue) / 4

Decoding of the each line info block - mono

Pixel

0

1

2

3

4

5

6

7

8

9

Mono

Continues line count

Continues line count

Speed to high / Line time

Line time

Encoder Clocks

Encoder Clocks

Encoder Clocks

State of external input line

Continues line count

This counter increments by 1 for each row of the image. The counter continues counting for new images and is not reset. It can be used to detect missing image information.

Structure

Continuous line count

Byte 1

Byte 0

Px1 (Content of Pixel Position 1)  

Px2

Decoding

The decoding of the continuous line count is:

Clc = Px1 × 256 + Px2

Line time

This information represents the line time. For an operation without a line trigger, this variable is constant and equal to the camera parameter line time. If the camera is triggered with a line trigger this information can be used to check the signal/mechanical transport quality.

  • If the signal oscillates very heavily with a high frequency the electrical connection is not OK.

  • Small oscillations (for example +-20%) are most probably mechanical vibrations in the transport process.
    These effects are typical for:

    • Belt drives

    • Conveyor belts

    • Low-quality linear stages for scans with a high resolution.

Structure

Line time

Byte 1

Byte 0

Px3

Px4

Decoding

The decoding of the line time is:

Lt = (Px3 × 28 + Px4 )× 25 / 100

Encoder clocks

24Bit encoder counter. Starts with Power on at 0 and overflows at 2^24. Counts, depending on the operating mode set, either the line trigger pulses or the encoder pulses. Can be used as location information of the document within the batch (sequence).

Can be reset via EnableIncremets(SelectEncoder(9:7)).

Structure

Encoder clocks

Byte 2

Byte 1

Byte 0

Px5

Px6

Px7

Decoding

The decoding of the encoder clocks is:

Ec = Px5 × 216 + Px6 × 28 + Px7

State of external Inputs

Structure

State of external Inputs

Byte 0

Px8

Output List

Line

Output Signal in Pixel position 8

Line1

8

Line2

9

Line3

10

Line4

11

Line5

12

Line6

13

Line7

14

Line8

15

Decoding

The decoding of the encoder clocks is:

Ei = Px8