Documentation Index

Fetch the complete documentation index at: https://docs-linescan.alliedvision.com/llms.txt

Use this file to discover all available pages before exploring further.

Modifying and showing features

Prev Next

Modifying features

GCT allowed to modify the features in two different ways. On the one hand, the configuration panel makes setting functions more convenient, special views show a set of related functions on which you can easily change these parameters. On the other hand, the camera feature panel allowed to edit the parameter in the XML-Tree.

In the Configuration panel

The view consists of four main tabs Acquisition Control, Camera Image Calibration, Pixel Processing and Special functions. Each tab shows several subtabs.

The Acquisition Control tab, for example, show five subtabs, which permit to specify many features such as image format and trigger settings. Some features also have additional explanation pictures.

in-the-configuration-panel-image-nsxbu0ka

In the camera feature panel (XML Tree)

On the left side of the GCT window, features and their values are shown in a tree structure organized in feature groups. To show the features of a feature group, click on the arrow preceding the group name.

in-the-camera-feature-panel-xml-tree-image-0dq1ofnj

Modifying features

In the configuration panel, the information is displayed when you move the mouse pointer over the parameter input field or the blue information icon.

Showing feature details

Feature details can be displayed in the configuration panel and in the camera feature panel.

In the Configuration panel

In the configuration panel, the information is displayed when you move the mouse pointer over the parameter input field or the blue information icon.

in-the-configuration-panel-image-sghpa627

in-the-configuration-panel-image-d7jggcwd