Safety instructions
Only technicians of Allied Vision Konstanz GmbH are permitted to open or slacken screws or housing sections of the device.
Before carrying out any work on the device disconnect the power supply.
To avoid the risk of fire let other devices such as radiators, heaters or lightning equipment cool down first.
Necessary repairs may only be carried out by Allied Vision Konstanz GmbH.
![]() | CAUTION |
| The device can heat up to 60 °C. | |
| Do not touch the hot surface. Let the device cool down before carrying out any work on it. |
Cleaning
During operation of the device, particles such as dust etc. may be settled on the lens. These deposits affect the quality of the optical image and the function of the device negatively.
Cleaning intervals
Specify regular cleaning intervals depending on your ambient conditions and the degree of soiling.
Cleaning procedure
Disconnect the power supply.
Let the device cool down.
Wipe all surfaces with a soft and lint-free cloth, starting with the lens. The use of isopropanol ist optional, refer to the manufacturer's manual.
Inspect the device to ensure that cleaning was effective and repeat if necessary.
Repair
In case of damages to the device refer to Allied Vision Konstanz GmbH.
Disposal
| This product is an electronic device. |

CAUTION