![]() | WARNING |
| The device can heat up to 75 °C. | |
| Do not touch the hot surface. Let the device cool down before carrying out any work on it. |
Safety instructions
- Only technicians of Allied Vision GmbH are permitted to open or slacken screws or housing sections of the device.
- Inform all persons working on the machine or system before carrying out any work on the device.
- Disconnect the power supply before carrying out any work on the device.
- To avoid the risk of fire let the device and other devices such as radiators or heaters cool down.
- Do not immerse the device in cleaning liquid or pour cleaning liquid over the device.
- Always use a soft cleaning cloth.
- Necessary repairs may only be carried out by Allied Vision GmbH.
Cleaning
During operation of the device particles such as dust can decrease the performance.
Cleaning intervals
Specify regular cleaning intervals depending on your ambient conditions and the degree of soiling.
Check the device for visible external damage before cleaning.
Cleaning procedure
![]() | |
| Risk of fire when using isopropanol as cleaning liquid | |
| Follow the safety instructions in the manufacturer's safety datasheet. |
| NOTICE | |
| Damage to the acrylic screen | |
When using the more fragile acrylic screen refer to the following safety instructions:
Do NOT use:
|
There is no need to remove parts of the device for cleaning.
- Disconnect the power supply.
- Let the device cool down.
- Clean the housing and the front glass of the light with a soft, moist and lint-free cloth. The use of isopropanol as a cleaning liquid for the front glass is optional, refer to the manufacturer's manual.
- Inspect the device to ensure that cleaning was effective and repeat if necessary.
Repairing
| NOTICE | |
| Irreparable damage to the device | |
| The device may only be opened by technicians of Chromasens GmbH. |
In case of damages to the device refer to Allied Vision GmbH. Before returning the device for repair contact the Allied Vision support and ask for a RMA number.
Disposal
![]() | This product is an electronic device. Please dispose this product in accordance with your local regulations. Contact your local government office for details about environmentally safe recycling. |

.png)