Interface specifications
Front side of the XLC4 control unit | |
1 | X4 Power supply input |
2 | X5 Analog control/shutdown/VOUT |
3 | X6 PWM interface/external switch |
4 | X1 RS232 connector |
5 | X7 RS485 interface |
6 | X2 USB connector |
7 | X3 Ethernet connector |
Rear side of the XLC4 control unit | |
1 | X8 LED output channel |
2 | X9 LED output channel |
3 | green status LED |
4 | yellow status LED |
5 | red status LED |
6 | X10 LED output channel |
7 | X11 LED output channel |