Documentation Index

Fetch the complete documentation index at: https://docs-linescan.alliedvision.com/llms.txt

Use this file to discover all available pages before exploring further.

Set exposure time

Prev Next
Note 
The exposure time must be smaller than the Acquisition Line Time plus an offset.
The minimum difference between the Acquisition Line Time and the Exposure Time is camera variant specific. Therefore, query the min and max entries of this feature. 

In the Configuration window navigate to Acquisition ControlExposure.

8k sensor

Common exposure time

  1. In Exposure time mode select Common.
  2. Set one exposure time for all sensor lines.
camera-features-image-k0nowbgg

Individual exposure time

  1. In Exposure time mode select Individual.
  2. Set an individual exposure time for each sensor line.
camera-features-image-7e9p4pl0

15k and 10k sensor

Common exposure time

The 15k and 10k sensors only support one common exposure time.