csiAcquistionStatistics Struct Reference
Structure containing acquisition statistics.
#include <csi/csi.h>
Collaboration diagram for csiAcquistionStatistics:

Data Fields
int64_t framesUnderrun
int64_t framesDropped
int64_t framesAcquired
int64_t networkPacketsOK
int64_t networkPacketsError
Detailed Description
Structure containing acquisition statistics.
Note
Negative statistic values indicate that they are not available.
Field Documentation
int64_t framesAcquired
Total number of frames acquired in current acquisition.
int64_t framesDropped
Number of frames dropped during acquisition.
int64_t framesUnderrun
The number of frames that were received in the TL but not send to the application because of missing buffers.
int64_t networkPacketsError
For GigE Vision: The number of network packets sent with an error.
int64_t networkPacketsOK
For GigE Vision: The number of network packets received without errors..
The documentation for this struct was generated from the following file:
csi.h
csiCalibrationParams Struct Reference
Structure containing calibration parameters.
#include <csi/csi.h>
Collaboration diagram for csiCalibrationParams:

Data Fields
bool enableROI
int64_t yStartROI
int64_t heightROI
bool enableExtrapolationLeft
bool enableExtrapolationRight
int64_t extrapolationLeft
int64_t extrapolationRight
int64_t extrapolationWidth
uint64_t firstValidPixel
int64_t targetValue
bool calcImprove
double contrast
double brightness
bool isCCDSensor = false
Detailed Description
Structure containing calibration parameters.
Field Documentation
double brightness
Brightness value for calibration.
bool calcImprove
double contrast
Contrast value for calibration.
bool enableExtrapolationLeft
To enable/disable extrapolation based PRNU calibration generation on the left side of the image.
bool enableExtrapolationRight
To enable/disable extrapolation based PRNU calibration generation on the right side of the image.
bool enableROI
To enable ROI based PRNU calibration data generation.
int64_t extrapolationLeft
The first column on the left side of the image that starts the extrapolation area in left side.
int64_t extrapolationRight
The last column on the right side of the image that ends the extrapolation area in right side.
int64_t extrapolationWidth
The width of the extrapolation area on both left and right side.
uint64_t firstValidPixel
Pixel offset of the loaded image.Start position of first valid pixel.In firmware version older than 2.2.0, the first pixel has default offset 1. In firmware 2.2.0 or newer,the first pixelhas default offset value 0.
int64_t heightROI
Height of the ROI used for PRNU calibration generation.
bool isCCDSensor = false
For CCD Sensors, the extrapolation process is done differently than for CMOS sensors (All GigE and CXP-based Allied Vision cameras).
int64_t targetValue
For PRNU, the target value of the resultant pixel value. Example, the max value of 8 bit pixel is 255.
int64_t yStartROI
The row number of the source image which is the beginning of ROI.
The documentation for this struct was generated from the following file:
csi.h
csiDataStreamInfo Struct Reference
Structure containing data stream infomation.
#include <csi/csi.h>
Collaboration diagram for csiDataStreamInfo:

Data Fields
char identifier [CSI_INFO_STRING_BUFFER_SIZE]
char displayName [CSI_INFO_STRING_BUFFER_SIZE]
uint32_t index
Detailed Description
Structure containing data stream infomation.
Field Documentation
char displayName[CSI_INFO_STRING_BUFFER_SIZE]
Display name of a data stream that can be used for GUI representation
char identifier[CSI_INFO_STRING_BUFFER_SIZE]
Unique identifier of a data stream
uint32_t index
Internal index of the data stream
The documentation for this struct was generated from the following file:
csi.h
csiDeviceInfo Struct Reference
Structure containing detailed device information.
#include <csi/csi.h>
Collaboration diagram for csiDeviceInfo:

Data Fields
char deviceIdentifier [CSI_INFO_STRING_BUFFER_SIZE]
char name [CSI_INFO_STRING_BUFFER_SIZE]
char model [CSI_INFO_STRING_BUFFER_SIZE]
char vendor [CSI_INFO_STRING_BUFFER_SIZE]
char serialNumber [CSI_INFO_STRING_BUFFER_SIZE]
char interfaceDescription [CSI_INFO_STRING_BUFFER_SIZE]
char interfaceID [CSI_INFO_STRING_BUFFER_SIZE]
char userName [CSI_INFO_STRING_BUFFER_SIZE]
char version [CSI_INFO_STRING_BUFFER_SIZE]
int64_t cameraSwPackageIsConsistent
csiTLProducerInfos tlProducerInfos
csiDeviceAccessStatus accessStatus
uint64_t timestampFrequediscncy
Detailed Description
Structure containing detailed device information.
Field Documentation
csiDeviceAccessStatus accessStatus
The current access status of the device, see csiDeviceAccessStatus
int64_t cameraSwPackageIsConsistent
char deviceIdentifier[CSI_INFO_STRING_BUFFER_SIZE]
Unique identifier of the device
char interfaceDescription[CSI_INFO_STRING_BUFFER_SIZE]
Name or description of the interface the device is connected to
char interfaceID[CSI_INFO_STRING_BUFFER_SIZE]
Unique identifier of the interface the device is connected to
char model[CSI_INFO_STRING_BUFFER_SIZE]
char name[CSI_INFO_STRING_BUFFER_SIZE]
char serialNumber[CSI_INFO_STRING_BUFFER_SIZE]
uint64_t timestampFrequediscncy
Frequency of the timestamps coming from the device
csiTLProducerInfos tlProducerInfos
Information about the transport layer the device is connected to
char userName[CSI_INFO_STRING_BUFFER_SIZE]
Username when opening the device
char vendor[CSI_INFO_STRING_BUFFER_SIZE]
char version[CSI_INFO_STRING_BUFFER_SIZE]
The documentation for this struct was generated from the following file:
csi.h
csiDiscoveryInfo Struct Reference
Structure containing information about device discovery.
#include <csi/csi.h>
Collaboration diagram for csiDiscoveryInfo:

Data Fields
uint32_t numDevices
double progress
bool discoveryRunning
csiDeviceInfo devices [CSI_DISCOVERY_INFO_DEVICE_COUNT]
Detailed Description
Structure containing information about device discovery.
Field Documentation
csiDeviceInfo devices[CSI_DISCOVERY_INFO_DEVICE_COUNT]
A list of devices found so far. The number of the devices found might exceed the size of this list, in which case the information must be acquired using the csiGetDeviceInfo() function.
bool discoveryRunning
Indicates if the discovery is still ongoing (true) or finished (false)
uint32_t numDevices
Current number of devices found during discovery
double progress
The documentation for this struct was generated from the following file:
csi.h
csiDownloadParams Struct Reference
Structure containing Download parameters and options.
#include <csi/csi.h>
Collaboration diagram for csiDownloadParams:

Data Fields
csiFileTransferParams fileParams
csiDownloadOptions options
Detailed Description
Structure containing Download parameters and options.
Field Documentation
csiFileTransferParams fileParams
csiDownloadOptions options
The documentation for this struct was generated from the following file:
csi.h
csiEventData Struct Reference
Structure containing information about event.
#include <csi/csi.h>
Collaboration diagram for csiEventData:

Data Fields
csiEventType type
csiHandle sender
csiModuleLevel senderType
char * tl_rawEventData
size_t tl_rawEventDataSizeBytes
char * eventValue
size_t eventValueSizeBytes
uint64_t eventIdentifier
Detailed Description
Structure containing information about event.
Field Documentation
uint64_t eventIdentifier
char* eventValue
The received value that was shipped together with the event. This can be for example the image data or a error description text in case of an error event. How to interpret the value depends on the type of event.
size_t eventValueSizeBytes
Size of the eventValue member in bytes
csiHandle sender
Handle to the sender of the event
csiModuleLevel senderType
Module level of the sender handle, see csiModuleLevel
char* tl_rawEventData
Raw data pointer to the event data as it was sent by the producer. This is just the raw data of the event which contains information about the type of event itself and not the value behind the event. See eventValue to get the actual value (e.g., image data) behind the event, if any.
size_t tl_rawEventDataSizeBytes
Size of the eventData member in bytes
csiEventType type
Type of the event, see csiEventType
The documentation for this struct was generated from the following file:
csi.h
csiFeatureParameter Struct Reference
Structure containing information about raw feature parameter.
#include <csi/csi.h>
Collaboration diagram for csiFeatureParameter:

Data Fields
csiFeatureType type
csiFeatureVisibility visibility
csiAccessMode access
csiDisplayNotation displayNotation
csiRepresentation representation
char displayPrecision
int64_t valueInt
int64_t incrementInt
int64_t minimumInt
int64_t maximumInt
int64_t validValueSetInt [CSI_INFO_INT_BUFFER_SIZE]
size_t validValueSetSizeInt
double valueFlt
double incrementFlt
double minimumFlt
double maximumFlt
char valueStr [CSI_INFO_STRING_BUFFER_SIZE]
size_t maximumStringLength
int64_t level
uint32_t enumCounter
int32_t enumIndex
char displayName [CSI_INFO_STRING_BUFFER_SIZE]
char name [CSI_INFO_STRING_BUFFER_SIZE]
char tooltip [CSI_INFO_STRING_BUFFER_SIZE]
char valueUnit [CSI_INFO_STRING_BUFFER_SIZE]
size_t featureRegLength
int64_t featureRegAddress
bool isFeature
bool isLittleEndian
Detailed Description
Structure containing information about raw feature parameter.
Field Documentation
csiAccessMode access
How a feature can be accessed, see csiAccessMode
char displayName[CSI_INFO_STRING_BUFFER_SIZE]
Display name of the feature for UI display
csiDisplayNotation displayNotation
How to display floating point features, see csiDisplayNotation. (Optional)
char displayPrecision
Precision of floating-point value representation
uint32_t enumCounter
Number of elements in the enumeration feature
int32_t enumIndex
The index of an enumeration entry
int64_t featureRegAddress
size_t featureRegLength
double incrementFlt
Possible increment for the feature value, in case of floating-point feature type
int64_t incrementInt
Possible increment for the feature value, in case of integer feature type
bool isFeature
bool isLittleEndian
int64_t level
The level of a feature in the tree (for graphical representation)
double maximumFlt
Maximum for the feature value, in case of floating-point feature type
int64_t maximumInt
Maximum for the feature value, in case of integer feature type
size_t maximumStringLength
Maximum length of the string feature value
double minimumFlt
Minimum for the feature value, in case of floating-point feature type
int64_t minimumInt
Minimum for the feature value, in case of integer feature type
char name[CSI_INFO_STRING_BUFFER_SIZE]
The name that identifies a feature
csiRepresentation representation
How feature data should be represented, see csiRepresentation (Optional)
char tooltip[CSI_INFO_STRING_BUFFER_SIZE]
Additional information about the feature that can be shown as tooltip in a GUI
csiFeatureType type
Data type of the feature, see csiFeatureType
int64_t validValueSetInt[CSI_INFO_INT_BUFFER_SIZE]
size_t validValueSetSizeInt
double valueFlt
Value of the feature, in case of floating-point feature type
int64_t valueInt
Value of the feature, in case of integer feature type
char valueStr[CSI_INFO_STRING_BUFFER_SIZE]
Value of the feature, in case of string feature type
char valueUnit[CSI_INFO_STRING_BUFFER_SIZE]
String unit to append to the value representation in a GUI
csiFeatureVisibility visibility
The visibility of a feature, see csiFeatureVisibility
The documentation for this struct was generated from the following file:
csi.h
csiFileTransferParams Struct Reference
Structure containing file transfer parameter.
#include <csi/csi.h>
Collaboration diagram for csiFileTransferParams:

Data Fields
const char * fileName
const char * fileType
Detailed Description
Structure containing file transfer parameter.
Field Documentation
const char* fileName
const char* fileType
The documentation for this struct was generated from the following file:
csi.h
csiImageInfo Struct Reference
Structure containing information about captured image.
#include <csi/csi.h>
Collaboration diagram for csiImageInfo:

Data Fields
uint32_t width
uint32_t height
uint32_t linePitch
uint32_t numChannels
csiPixelFormat format
Detailed Description
Structure containing information about captured image.
Field Documentation
csiPixelFormat format
Pixel format of the image data, see csiPixelFormat
uint32_t height
uint32_t linePitch
Line pitch of the image data in bytes
uint32_t numChannels
uint32_t width
The documentation for this struct was generated from the following file:
csi.h
csiMemTransferInfo Struct Reference
Structure containing information about memory transfer.
#include <csi/csi.h>
Collaboration diagram for csiMemTransferInfo:

Data Fields
csiHandle device
size_t totalBytesToTransfer
size_t bytesTransferred
csiMemTransferStatus status
csiErr errorCode
const char * progressText
Detailed Description
Structure containing information about memory transfer.
Field Documentation
size_t bytesTransferred
Current number of bytes already transferred.
csiHandle device
Handle to the device where the transfer is running on.
csiErr errorCode
Error code in case an error occurred.
const char* progressText
csiMemTransferStatus status
Status of the memory transfer, see csiMemTransferStatus.
size_t totalBytesToTransfer
Total number of bytes to be transferred.
The documentation for this struct was generated from the following file:
csi.h
csiNewBufferEventData Struct Reference
Structure containing data of an incoming buffer event.
#include <csi/csi.h>
Collaboration diagram for csiNewBufferEventData:

Public Member Functions
csiNewBufferEventData ()
~csiNewBufferEventData ()
csiNewBufferEventData (const csiNewBufferEventData &other)
csiNewBufferEventData (csiNewBufferEventData &&other) noexcept
csiNewBufferEventData & operator= (csiNewBufferEventData &other)
csiNewBufferEventData & operator= (csiNewBufferEventData &&other) noexcept
Data Fields
csiEventType type { CSI::csiEventType::CSI_EVT_NEWIMAGEDATA }
csiHandle sender { CSI_EMPTY_HANDLE }
csiModuleLevel senderType { CSI::csiModuleLevel::CSI_UNKNOWN_MODULE }
char * tl_rawEventData { nullptr }
size_t tl_rawEventDataSizeBytes { 0 }
unsigned char * eventValue { nullptr }
size_t eventValueSizeBytes { 0 }
uint64_t eventIdentifier { 0 }
csiHandle bufferHandle { 0 }
uint64_t imageNr { 0 }
uint64_t bufferIdentifier { 0 }
uint64_t timestampMS { 0 }
uint64_t timestampRaw { 0 }
csiImageInfo imageInfo {}
Detailed Description
Structure containing data of an incoming buffer event.
Constructor & Destructor Documentation
csiNewBufferEventData ()
~csiNewBufferEventData ()
csiNewBufferEventData (const csiNewBufferEventData & other)
csiNewBufferEventData (csiNewBufferEventData && other)[noexcept]
Member Function Documentation
csiNewBufferEventData & operator= (csiNewBufferEventData && other)[noexcept]
csiNewBufferEventData & operator= (csiNewBufferEventData & other)
Field Documentation
csiHandle bufferHandle { 0 }
Handle to the buffer holding the image (for internal use)
uint64_t bufferIdentifier { 0 }
Unique identifier of the image, usually the pointer as integer representation
uint64_t eventIdentifier { 0 }
Unique identifier of this event
unsigned char* eventValue { nullptr }
size_t eventValueSizeBytes { 0 }
Size of the image data in bytes
csiImageInfo imageInfo {}
Further image information, see csiImageInfo
uint64_t imageNr { 0 }
csiHandle sender { CSI_EMPTY_HANDLE }
Sender of the event, a stream handle
csiModuleLevel senderType { CSI::csiModuleLevel::CSI_UNKNOWN_MODULE }
Type of the sender, this is always CSI_STREAM_MODULE for this type of event
uint64_t timestampMS { 0 }
Timestamp of the image in milliseconds
uint64_t timestampRaw { 0 }
char* tl_rawEventData { nullptr }
Raw data pointer to the event data as it was sent by the producer. This is just the raw data of the event which contains information about the type of event itself and not the value behind the event. See eventValue to get the actual value (e.g., image data) behind the event, if any.
size_t tl_rawEventDataSizeBytes { 0 }
Size of the eventData member in bytes
csiEventType type { CSI::csiEventType::CSI_EVT_NEWIMAGEDATA }
Type of the event, this is always CSI_EVT_NEWIMAGEDATA for this type of event
The documentation for this struct was generated from the following file:
csi.h
csiTLInterfaceDiscoveryInfo Struct Reference
Structure containing information about transport layer interface discovery.
#include <csi/csi.h>
Collaboration diagram for csiTLInterfaceDiscoveryInfo:

Data Fields
uint32_t numInterfaces
double progress
bool discoveryRunning
csiTLInterfaceInfo interfaceInfos [CSI_TL_INTERFACE_COUNT]
Detailed Description
Structure containing information about transport layer interface discovery.
Field Documentation
bool discoveryRunning
Indicates if the discovery is still ongoing (true) or finished (false)
csiTLInterfaceInfo interfaceInfos[CSI_TL_INTERFACE_COUNT]
A list of TL interfaces found so far.
uint32_t numInterfaces
double progress
The documentation for this struct was generated from the following file:
csi.h
csiTLInterfaceInfo Struct Reference
Structure containing information about transport layer interface.
#include <csi/csi.h>
Collaboration diagram for csiTLInterfaceInfo:

Data Fields
char interfaceDescription [CSI_INFO_STRING_BUFFER_SIZE]
char interfaceID [CSI_INFO_STRING_BUFFER_SIZE]
csiTLProducerInfos tlProducerInfos
Detailed Description
Structure containing information about transport layer interface.
Field Documentation
char interfaceDescription[CSI_INFO_STRING_BUFFER_SIZE]
char interfaceID[CSI_INFO_STRING_BUFFER_SIZE]
csiTLProducerInfos tlProducerInfos
The documentation for this struct was generated from the following file:
csi.h
csiTLProducerInfos Struct Reference
Structure containing infomation about transport layer producer.
#include <csi/csi.h>
Collaboration diagram for csiTLProducerInfos:

Data Fields
char transportLayerName [CSI_INFO_STRING_BUFFER_SIZE]
char transportLayerDisplayName [CSI_INFO_STRING_BUFFER_SIZE]
char transportLayerType [CSI_INFO_STRING_BUFFER_SIZE]
char transportLayerPath [CSI_INFO_STRING_BUFFER_SIZE]
char transportLayerID [CSI_INFO_STRING_BUFFER_SIZE]
size_t pathSizeInBytes
Detailed Description
Structure containing infomation about transport layer producer.
Field Documentation
size_t pathSizeInBytes
Length of the transport layer path.
char transportLayerDisplayName[CSI_INFO_STRING_BUFFER_SIZE]
Display name of a transport layer for GUI representation.
char transportLayerID[CSI_INFO_STRING_BUFFER_SIZE]
Unique identifier of the transport layer as string.
char transportLayerName[CSI_INFO_STRING_BUFFER_SIZE]
char transportLayerPath[CSI_INFO_STRING_BUFFER_SIZE]
Full path to the transport layer library file (.cti file).
char transportLayerType[CSI_INFO_STRING_BUFFER_SIZE]
Type of the transport layer as string.
The documentation for this struct was generated from the following file:
csi.h
csiUploadParams Struct Reference
Structure containing Upload parameters and options.
#include <csi/csi.h>
Collaboration diagram for csiUploadParams:

Data Fields
csiFileTransferParams fileParams
csiUploadOptions options
Detailed Description
Structure containing Upload parameters and options.
Field Documentation
csiFileTransferParams fileParams
csiUploadOptions options
The documentation for this struct was generated from the following file:
csi.h