The control panel is displayed after connecting to a XLC4 control unit.
Overview control panel
Informative elements
| ||
1 | Current output voltage of LED output channel (X8, X9, X10, X11) | |
2 | Temperature of the XLC4 control unit and the Corona II module | |
3 | Serial number of the Corona II module | |
4 | Number of connected LED boards to the Corona II module | |
5 | Current input voltage (X4) | |
6 | Current operating mode | |
7 | Port name or IP address used by this tab | |
8 | Selected interface type for connection to the XLC4 control unit | |
9 | Firmware version of the XLC4 control unit | |
10 | Serial number of the XLC4 control unit | |
Functional elements
| |
1 | Checkbox on/off: Switch Corona II module on or off |
2 | Input box: Manually enter the LED current value |
3 | Button apply: Activate and store the new value for the LED current |
4 | Slider: Adjust the LED current value |
.png)
.png)