Configure multi-channel flash control

Prev Next

The camera can be used to trigger up to four different flash controller channels synchronized to their line acquisition. You can acquire several images with different illumination colors simultaneously in a single scan using line-multiplexing. The camera starts a complete LED pattern sequence after each line trigger or after a sequence time in free-running mode.

The multi flash setup

The setup contains two Corona II illuminations which are controlled by the camera.

svg-multi flash setup_03
1Line scan camera: scans the image line by line and communicates with the PC.2PC: performs subsequent processing of the image data and can control the illumination system.
3Illumination: lights up the scan area.4Illumination controller: controls and monitors the illumination unit.
5Speed detection: the encoder detects the speed of the conveyor belt and communicates with the camera.

Connect the camera with the XLC4 controller

Any flash controller compatible to the electrical and timing specifications of the camera output interface can be synchronized. For best compatibility use the Allied Vision illumination controller XLC4 (CP000411) illuminations from the Corona II product line.

Refer to the XLC4 controller manual.

Set up the flash controller

The camera provides up to four different outputs which can be operated individually to control flash controllers. Several flash outputs can be individually configured. 

Flash controller: basic mode

The basic mode is a sequential flash with up to four channels.

  1. In the Configuration window navigate to Special Functions → Flash Controller.
  2. Below Flash controller: basic setup mode select the Enable checkbox.
  3. Adjust the parameters to your needs.

Alternatively you can set up the basic flash controller in the camera feature tree by executing the following steps:

StepFeature nameValue
1Led Flash Control
Led Flash Enable
On
2Led Flash Number of Pattern<number of Pattern>
3Led Flash Pattern SelectorLed Flash Pattern <1>
4Out1 on Time<on time in µs>
5Pattern of Delay<delay time in µs>
6Led Flash Pattern SelectorLed Flash Pattern <n>
7Out-n on Time<on time in µs>
8Pattern of Delay<delay time in µs>
9Flash frame control–
10Led Flash sequence time–

Flash controller: advanced mode

The advanced mode is a sequential flash with up to four channels and four patterns for each channel. The patterns are executed in a sequence. The sequence is repeated as long as scanning or triggering is active.

  1. In the Configuration window navigate to Special Functions → Flash Controller.
  2. Scroll down to Flash controller - advanced setup mode.
  3. Below Flash controller - advanced setup mode select the Enable checkbox.
  4. Adjust the parameters to your needs.

In this example two flash patterns are selected. The duration for each line pattern is set individually. All output channels are used.

Alternatively you can set up the advanced flash controller in the camera feature tree by executing the following steps:

StepFeature nameValue
1Led Flash Control
Led Flash Enable
On
2Led Flash Number of Pattern<number of Pattern>
3Led Flash Pattern SelectorLed Flash Pattern <1>
4Out1 – 4 on Time <on time in µs>
5Pattern of Delay<delay time in µs>
6Led Flash Pattern SelectorLed Flash Pattern <n>
7Out1 – 4 on Time<on time in µs>
8Pattern of Delay<delay time in µs>
9Flash frame control–
10Led Flash sequence time–

Deinterlace the image

The following image shows how to separate the flash channels on an example of two flash channels.

svg-flash deinterlace image_03