Documentation Index

Fetch the complete documentation index at: https://docs-linescan.alliedvision.com/llms.txt

Use this file to discover all available pages before exploring further.

Check the image quality

Prev Next
  1. Place an image target under the camera, e.g. a colorchecker classic. 
  2. Acquire an image.
  3. Analyze the image: If the image is covered with vertical stripes you may have not used a moving shading reference.
getting-started-image-ytdldilj
  1. If the image has color shifts check the scan direction.
getting-started-image-1k2h7jgr
  1. If the image is compressed in transport direction adapt the encoder divider float value or the acquisition line rate.
getting-started-image-0frmta02
  1. If the image is shown mirror-inverted, use the ReserveX parameter.

getting-started-image-iri79ww0mirrored

This is an example of a good image quality.getting-started-image-iri79ww0