For alignment of the allPIXA camera with GCT software, an adjustment target is required.

Sample Adjustment Target
As each alignment target is unique regarding field of view and optical resolution, number of cameras an so on, the data for a customized alignment target must be created.
This can be performed using the Camera Configurator.
Camera Configurator - Target for camera adjustment
First insert the parameter in the in Camera Configurator and choose the fitting camera and lens. Selecting the tab Accessories and choose Target for camera adjustment.
Insert Text for ruler labeling and click Generate adjustment target.

Camera Configurator Target for camera adjustment
The Camera Configurator generates the following files:
PDF Printing template: Template for printing the adjustment target, please check required printing resolution.
DXF Production data: DXF File for target manufacturer, for high resolution targets, e.g. film photomasks.
Specification ruler: Ruler description as json.file to load into GCT2 Software. This file defines the position and dimensions of the markers on the target.
GCT Parameter: Parameter description as json.file to load into the GCT Software see also Parameter.
PDF Drawing with dimension: Reference document for verifying adjustment marker position and size on the target, facilitating discussion with the target manufacturer.
If the Camera Configurator does not get you a sufficient result, please email support-konstanz@alliedvision.com with the following details for assistance::
Field of View (single camera)
Optical resolution (camera)
Number of cameras
Overlapping area (multiple cameras)
Total Field of View (multiple cameras)"
The following options are available for purchasing the alignment target:
Use the provided PDF and DXF files to contact your preferred manufacturer to inquire about their products or services.
Reach out to Allied Vision Sales team or email support-konstanz@alliedvision.com to confirm availability of a suitable Linear Target product (CC03138-…).
Please note that due to the high variety of possible targets, Allied Vision cannot guarantee the availability of a specific target in every case.