--- title: "Electrical installation-A2" slug: "neo-electrical-installation" updated: 2025-10-14T14:16:58Z published: 2025-10-14T14:16:58Z canonical: "docs-linescan.alliedvision.com/neo-electrical-installation" --- > ## Documentation Index > Fetch the complete documentation index at: https://docs-linescan.alliedvision.com/llms.txt > Use this file to discover all available pages before exploring further. # Electrical installation ## GigE interface The 10 GigE connectors permit to use (direct attach) copper cables with lengths of up to 30 m (10BASE-T). A cable with the minimum specification of CAT6a must be used. ### Network adapter To establish a 10 GigE connection a network adapter with a 10 GigE RJ45 input must be installed and configured on the PC. The installation of the network adapter is explained in the GCT documentation. For more information, see [Installation GigE](/v1/docs/installation-gige). For more information about the tested network adapters and the transceivers, see [Tested Network adapters and Transceivers.](/v1/docs/tested-network-adapters-and-transceivers) ### Cabling | ![electricity](https://cdn.document360.io/eca58697-9c2f-461e-9f0a-e6205b74b693/Images/Documentation/electricity.png) | **![general warning](https://cdn.document360.io/eca58697-9c2f-461e-9f0a-e6205b74b693/Images/Documentation/general%20warning(2).png)WARNING** | | --- | --- | | **Electric shock due to improper connection to a power supply.** | | Use a 12 V – 24 V DC power supply. When using the digital I/O port as a power supply ensure the correct polarity. | 1. Connect the video output port. 2. Connect the digital I/O port. #### Option 1: Power over Ethernet (PoE) 1. Plug the Ethernet cable into the Power/PoE port (PoEOUT) of the PoE injector and into the video output port (RJ45) of your camera. 2. Connect another Ethernet cable to the Ethernet/data (DataIN) port of the injector and your network card. #### Option 2: Power supply of the digital I/O port To set up the wiring refer to section [Digital I/O port](https://docs.chromasens.de/docs/neo-electrical-installation#digital-io-port). Note the permitted input voltages: | | Nominal | Minimum | Maximum | | --- | --- | --- | --- | | Permitted voltages | 24 V | 12 V | 28 V | ## CXP interface The interface allows you to connect two CXP cables. Micro BNC (for CXP12) connectors for the camera and suitable connectors for the frame grabber are required. The maximum cable length is 35 m. ### Frame grabber To establish a CXP connection a frame grabber must be installed and configured on the PC. Refer to the manual of your frame grabber. For more information about the tested frame grabbers, see [Tested frame grabbers](/v1/docs/tested-frame-grabbers-1). ### Cabling | ![electricity](https://cdn.document360.io/eca58697-9c2f-461e-9f0a-e6205b74b693/Images/Documentation/electricity.png) | **![general warning](https://cdn.document360.io/eca58697-9c2f-461e-9f0a-e6205b74b693/Images/Documentation/general%20warning(2).png)WARNING** | | --- | --- | | **Electric shock due to improper connection to a power supply.** | | Use a 12 V – 24 V DC power supply. When using the digital I/O port as a power supply ensure the correct polarity. | 1. Connect the video output port. 2. Connect the digital I/O port. #### Option 1: Power over CoaXPress (PoC) To use the power-over-CXP function two connections are needed. #### Option 2: Power supply of the digital I/O port To set up the wiring refer to section [Digital I/O port](https://docs.chromasens.de/docs/neo-electrical-installation#digital-io-port). Note the permitted input voltages: | | Nominal | Minimum | Maximum | | --- | --- | --- | --- | | Permitted voltages | 24 V | 12 V | 28 V | ## Digital I/O port The following connector is required for the digital I/O port: - 15 pin HD D-Sub (female) ![neo-digital%20io%20port-v03](https://cdn.document360.io/eca58697-9c2f-461e-9f0a-e6205b74b693/Images/Documentation/neo-digital%20io%20port-v03.svg)Pin allocation D-Sub connector (male) of the camera You can configure the digital I/O port as RS422 or as single-ended input or output. It is also possible to configure one output as RS422 and the other output as single-ended. **RS422 configuration** | Pin | Line definition for RS422 configuration | Signal RS422 | Configuration proposal | | --- | --- | --- | --- | | 1 | Line 1 | In1+ | Encoder Source A, Line Start | | 2 | In1– | Encoder Source A\, Line Start\ | | 3 | Line 2 | In2+ | Encoder Source B, Fame Start, Frame Active | | 4 | In2– | Encoder Source B\, Fame Start\, Frame Active\ | | 5 | GND (Signals) | | Signals Ground | | 6 | Line 3 | In3+/Out3+ | Encoder Source A, Fame Start, Frame Active, Line Start, User Output3+, MS-In+ | | 7 | In3–/Out3– | Encoder Source A\, Fame Start\, Frame Active\, Line Start\, User Output3-, MS-In- | | 8 | Line 4 | In4+/Out4+ | Encoder Source A, Fame Start, Frame Active, Line Start, User Output4+, MS-Out+ | | 9 | In4–/Out4– | Encoder Source A\, Fame Start\, Frame Active\, Line Start\, User Output4-, MS-Out- | | 10 | GND (PWR) | | Camera Power Ground | | 11 | Line 5 | Out5+ | User Output5+ | | 12 | Out5– | User Output5- | | 13 | Line 6 | Out6+ | User Output6+ | | 14 | | User Output6- | | 15 | Vcc (PWR) | | Camera Power DC +12 V – +24 V | **Single-Ended (SE) configuration** The input threshold voltage can be configured globally to 3.3 V, 5 V, 12 V and 24 V. The Maximum input voltage is 28 V. The set voltage level is then active for all single ended inputs and outputs. | Pin | Line definition for Single-Ended configuration | Signal Single-Ended | Configuration proposal | | --- | --- | --- | --- | | 1 | Line 1 | In1 (3.3 V, 5 V, 12 V, 24 V) | Encoder Source A, Line Start | | 2 | -- | -- | -- | | 3 | Line 2 | In2 (3.3 V, 5 V, 12 V, 24 V) | Encoder Source B, Fame Start, Frame Active | | 4 | -- | -- | -- | | 5 | GND (Signals) | | Signals Ground | | 6 | Line 3 | In3 (3.3 V, 5 V, 12 V, 24 V) Out3 (3.3 V) | Encoder Source A, Fame Start, Frame Active, Line Start, User Output3+ | | 7 | -- | -- | -- | | 8 | Line 4 | In4 (3.3 V, 5 V, 12 V,24 V) Out4 (3.3 V) | Encoder Source A, Fame Start, Frame Active, Line Start, User Output4+ | | 9 | -- | -- | -- | | 10 | GND (PWR) | | Camera Power Ground | | 11 | Line 5 | In5 (3.3 V) Out5 (3.3 V) | LED Flash Out 3, User Output5 | | 12 | Line 7 | In7 (3.3 V) Out7 (3.3 V) | LED Flash Out 2, User Output7 | | 13 | Line 6 | In6 (3.3 V) Out6 (3.3 V) | LED Flash Out 0, User Output6 | | 14 | Line 8 | In8 (3.3 V) Out8 (3.3 V) | LED Flash Out 1, User Output8 | | 15 | Vcc (PWR) | | Camera Power DC +12 V – +24 V | The Datasheet of I/O Cable CP000722-X and its internal color configuration can be found here: [Datasheet CP000722](https://chromasens.de/sites/default/files/download-media/TDS_CP000722-5.0-C_R02.pdf). ### Configure the I/O's The IO Ports can be configured in GCT. | 1. Connect and open the camera in GCT | | | --- | --- | | 2. Navigate to *Camera Features, Digital IO Control* | | | 3. Select the Line in the *Line Selector* | | | 4. Open the Drop-down menu and change the **Line Format** | ![](https://cdn.document360.io/eca58697-9c2f-461e-9f0a-e6205b74b693/Images/Documentation/image-1697630442352.png) | ### Circuit Diagrams #### RS422 configuration ![svg-neo-circuit_diagram_rs422](https://cdn.document360.io/eca58697-9c2f-461e-9f0a-e6205b74b693/Images/Documentation/svg-neo-circuit_diagram_rs422.svg)External circuit: RS422 device #### Single-Ended configuration ![svg-neo-circuit_diagram_1](https://cdn.document360.io/eca58697-9c2f-461e-9f0a-e6205b74b693/Images/Documentation/svg-neo-circuit_diagram_1.svg)External circuit: Optocoupler ![svg-neo-circuit_diagram_2](https://cdn.document360.io/eca58697-9c2f-461e-9f0a-e6205b74b693/Images/Documentation/svg-neo-circuit_diagram_2.svg)External circuit: TTL or CMOS logic gate ### Power supply To set up the wiring refer to section [Digital I/O port](https://docs.chromasens.de/docs/neo-electrical-installation#digital-io-port). Note the permitted input voltages: | | Nominal | Minimum | Maximum | | --- | --- | --- | --- | | Permitted voltages | 24 V | 12 V | 28 V | The input current is 0.5 A @ 24 V. Connection with one 10 GigE lane. Gigabit Ethernet (GigE) enables easy connection of industrial cameras. CoaXPress (CXP) is an asymmetric high-speed point-to-point serial communication standard for the transmission of video and still images, scalable over single or multiple coaxial cables.