--- title: "Command FA" slug: "command-fa" updated: 2024-07-04T11:08:16Z published: 2024-07-04T11:08:16Z canonical: "docs-linescan.alliedvision.com/command-fa" --- > ## Documentation Index > Fetch the complete documentation index at: https://docs-linescan.alliedvision.com/llms.txt > Use this file to discover all available pages before exploring further. # Command FA Command FA is used to set the content of the control register *“ControlFlagsA”.* ## Structure | Command | Notes | | --- | --- | | CommandID | FA | Only available in Command mode | | Parameter | None | | | | Register value | HexChar | | Parameter | Value | Description | | None | | The current value is queried | | Register value | 0x0000 | | Default value | | 0x0001 | Service | For service use only – set to 0 | | 0x0002 | Internal | For internal use only – set to 0 | | 0x0004 | ActSW | XLC4-1 and XLC4-1A: Activate use of Switch (SW1 to SW2 at connector X6) | | 0x0008 | ActVO | Activate use of VOUT (VOUT at connector X5) | | 0x0010 | CheckFan | Supervise Fan-valid signal (ACNTRL at connector X5) | | 0x0020 | Enable ON | Activates flash function (Signal ON at connector X6) | | 0x0200 | Channel control mode | XLC4-1F4: All channels are controlled independent from the inputs at X6 | | Response | | | fa , space , register value | | General notes | | | The register value is applied after switching on again. Combinations of single flags are possible. | ## Example with Register value | Query | Response | | --- | --- | | FA 0x000C | fa 0x000C | Activates VOUT and SW1-SW2 for cooling device. | ControlFlagA HexChar | Reserved | Reserved | EnableON | CheckFan | ActVO | ActSW | Internal use | Service | Description | | --- | --- | --- | --- | --- | --- | --- | --- | --- | --- | | 0x0000 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | ON disabled, no FAN control or external cooling device control | | 0x0004 | 0 | 0 | 0 | 0 | 0 | 1 | 0 | 0 | ON disabled, Standard mode with cooling device at SW1-SW2 | | 0x0008 | 0 | 0 | 0 | 0 | 1 | 0 | 0 | 0 | ON disabled, Standard mode with Fan at VOUT | | 0x000C | 0 | 0 | 0 | 0 | 1 | 1 | 0 | 0 | ON disabled, VOUT and SW1-SW2 active for cooling device | | 0x0020 | 0 | 0 | 1 | 0 | 0 | 0 | 0 | 0 | Switching XLC4 with ON-Input - no cooling device connected | | 0x0024 | 0 | 0 | 1 | 0 | 0 | 1 | 0 | 0 | Switching XLC4 with ON-Input - cooling device at SW1-SW2 | | 0x0028 | 0 | 0 | 1 | 0 | 1 | 0 | 0 | 0 | Switching XLC4 with ON-Input - Fan at VOUT | | 0x002C | 0 | 0 | 1 | 0 | 1 | 1 | 0 | 0 | Switching XLC4 with ON-Input - VOUT and SW1-SW2 active for cooling device | | 0x0018 | 0 | 0 | x | 1 | 1 | x | 0 | 0 | Activating the fan monitoring functions |