--- title: "Tested Network adapters and Transceivers" slug: "tested-network-adapters-and-transceivers" updated: 2025-04-14T11:26:00Z published: 2025-04-14T11:26:00Z canonical: "docs-linescan.alliedvision.com/tested-network-adapters-and-transceivers" --- > ## Documentation Index > Fetch the complete documentation index at: https://docs-linescan.alliedvision.com/llms.txt > Use this file to discover all available pages before exploring further. # Network adapters and transceivers ## SFP+ connection Note If you are using the s2i Transport Layer it is required to configure the network adapter properly. The **HPE Ethernet 10Gb 2-port 560SFP+ Adapter** and **Intel (X710)** are configured during installation. * Some manufacturers encode their cards. Those cards can only be used with the appropriate transceivers. Example: Intel X710 chipsets only work with Intel or Intel-configured transceivers ### Network adapter The following network adapters are tested with GCT2. The results are shown in the following table. | Vendor Name | Type | Result | S2i TL | Kithara TL | | --- | --- | --- | --- | --- | | HPE | HPE Ethernet 10Gb 2-port 560SFP+ Adapter | Fully functional | X | X | | HPE * | HPE Ethernet 10Gb 2-port 562SFP+ Adapter | Not supported yet | | | | Intel * | Intel® Ethernet-Converged-Network-Adapter X710 | Fully functional | X | X | | Myricom | Myricom 2x 10GbE SFP+ low-profile NIC | Only with s2i | X | | | Myricom | Myricom 1x 10GbE SFP+ low-profile NIC | Only with s2i | X | | | Mellanox | NVIDIA Mellanox MCX512A-ACAT ConnectX®-5 EN Network adapter | Only with s2i | X | | | Broadcom | P210P - 2 x 10GbE PCIe NIC | Only with s2i | x | | | Zebra | GevIQ | Fully functional | Zebra TL | #### Installation | Network adapter | | | --- | --- | | HPE Ethernet 10Gb 2-port 560SFP+ Adapter | Download and install the following files Download the *Wired_dirver_xx* and the *Wired_PROSet_xx from the* [*Intel Homepage*](https://www.intel.com/content/www/us/en/download/18293/intel-network-adapter-driver-for-windows-10.html)*.* | | Network adapter with X550 Intel chipset | Download and install the following files Download the *Wired_dirver_xx* and the *Wired_PROSet_xx from the* [*Intel Homepage*](https://www.intel.com/content/www/us/en/download/18293/intel-network-adapter-driver-for-windows-10.html)*.* | | Network adapter with X710 Intel chipset | Download and install the following files Download the Release_xx *from the* [*Intel Homepage*](https://www.intel.de/content/www/de/de/download/15084/intel-ethernet-adapter-complete-driver-pack.html)*.* | | Broadcom P210P | > [!NOTE] > Download an install the following files > > Download the Release_xx from the [Broadcom Homepage](https://www.broadcom.com/products/ethernet-connectivity/network-adapters/p210p) | | Zebra GevIQ | Download and install the following files Download the Release_xx from the [Zebra Homepage.](https://www.zebra.com/us/en/support-downloads/software/industrial-machine-vision-and-fixed-scanners-software/aurora/aurora-imaging-library.html) | ### Transceiver The following transceivers are tested with the allPIXA evo camera and the network adapters. | Vendor Name | Type | Comment | Camera side | Network adapter side | | --- | --- | --- | --- | --- | | Finisar | FTLX8574D3BCL Class 1 21CFR1040:10 | | X | X | | FS | SFP-10GSR-85 | | X | X | | FS | Intel E10GSFPSRX Compatible 10GBASE-SR SFP+ 850nm 300m DOM Duplex LC MMF Transceiver Module | Recommended for Network adapters that are marked with * | | X | ## RJ45 connection ### Network adapter The following network adapters are tested with GCT2. The results are shown in the following table. | Vendor name | Type | Result | s2i TL | Kithara TL | | --- | --- | --- | --- | --- | | Broadcom | P210TP - 2 x 10GBASE-T PCIe NIC | Fully functional | X | | ### Installation | 1. Download the driver file and follow the installation instructions. | Download For the Broadcom Network adapter "P210TP - 2 x 10GBASE-T PCIe NIC", you can find the download files [here](https://www.broadcom.com/products/ethernet-connectivity/network-adapters/p210tp). | | --- | --- |