--- title: "Synchronizing cameas: Master Slave operation" slug: "synchronize-the-cameras-master-slave-operation" updated: 2026-09-02T05:49:31Z published: 2026-09-02T05:49:31Z canonical: "docs-linescan.alliedvision.com/synchronize-the-cameras-master-slave-operation" --- > ## Documentation Index > Fetch the complete documentation index at: https://docs-linescan.alliedvision.com/llms.txt > Use this file to discover all available pages before exploring further. # Set up master slave operation The master slave mode synchronizes a master camera with several slave cameras. The frame trigger and line trigger are only connected to the master camera. The trigger information and additional timing signals are transferred to the slave cameras via the master-slave interface. All cameras run with exactly the same timing for lines and optional frames. ## Set up the master camera | 1. In the Configuration window navigate to *Special Functions* → *Master/Slave*. 2. Select the **Enable** checkbox. 3. In *Camera role* select the defined camera as **Master**. 4. In *Interface* select **External**. | ![](https://cdn.document360.io/eca58697-9c2f-461e-9f0a-e6205b74b693/Images/Documentation/camera-features-image-taioos9o.png) | | --- | --- | Alternatively you can set the camera as the master camera in the camera feature tree by executing the following steps: | Step | Feature name | Value | | --- | --- | --- | | 1 | Master Slave Mode | Master | | 2 | Master Slave Interface | External | | 3 | Maste Slave Interface Enable | On | ## Set up the slave camera | 1. In the Configuration window navigate to *Special Functions* → *Master/Slave*. 2. Select the **Enable** checkbox. 3. In *Camera role* select the defined camera as **Slave**. 4. In *Interface* select **External**. 5. As an option in *Slave camera settings* set the **frame trigger delay**. | ![](https://cdn.document360.io/eca58697-9c2f-461e-9f0a-e6205b74b693/Images/Documentation/camera-features-image-vzo8medq.png) | | --- | --- | Alternatively you can set the camera as the slave camera in the camera feature tree by executing the following steps: | Step | Feature name | Value | | --- | --- | --- | | 1 | Master Slave Mode | Slave | | 2 | Master Slave Interface | External | | 3 | Maste Slave Interface Enable | On | | 4 | Master Slave Delay Lines | | ## Connect master and slave camera The master/slave interface consists of a single timing signal for standard setup. Use suitable Allied Vision cables: | Cable type | Order number | | --- | --- | | Master Slave Hub cable allPIXA evo (0.5 m and 1.0 m) | CP000715 | | Trigger Cable allPIXA evo (5 m) | CP000716 | The connection is established through the digital I/O interface. 1. Connect **pin 14 (line 9)** of the master camera to **pin 8 (line 4)** of the slave camera. 2. Connect **pin 13 (GND)** of the master camera to **pin 13 (GND)** of the slave camera.