--- title: "Set the LED current" slug: "set-led-current" updated: 2024-07-03T13:44:32Z published: 2024-07-04T11:12:36Z canonical: "docs-linescan.alliedvision.com/set-led-current" stale: true --- > ## Documentation Index > Fetch the complete documentation index at: https://docs-linescan.alliedvision.com/llms.txt > Use this file to discover all available pages before exploring further. # Set the LED current You can adjust the current of the LED output channels. > [!NOTE] > NOTE > > This function does not save the new value for the current permanently. If you wish to save it permanently, use the [command IY](/v1/docs/command-iy). ## Set global LED current 1. In the general dropdown menu click **Channels**. 2. Click **Set global LED current**. ![](https://cdn.document360.io/eca58697-9c2f-461e-9f0a-e6205b74b693/Images/Documentation/image(69).png) A dialog window opens. ![](https://cdn.document360.io/eca58697-9c2f-461e-9f0a-e6205b74b693/Images/Documentation/image(68).png) 1. Set the desired current. Type the value in the input box or use the slider. 2. Click **OK**. ## Set individual LED current 1. In the *control panel* either type the value in the input box or use the slider. 2. Click **apply**. ![](https://cdn.document360.io/eca58697-9c2f-461e-9f0a-e6205b74b693/Images/Documentation/image(70).png)