--- title: "New releases allPIXA evo" slug: "releases" updated: 2026-07-15T13:19:48Z published: 2026-07-15T13:19:48Z canonical: "docs-linescan.alliedvision.com/releases" --- > ## Documentation Index > Fetch the complete documentation index at: https://docs-linescan.alliedvision.com/llms.txt > Use this file to discover all available pages before exploring further. # New releases allPIXA evo ## Release Overview allPIXA evo ### Release 13.0.0 (July 2026) | Camera | Release Notes | | --- | --- | | allPIXA evo 32k CXP | **Changes and New features** - Internal refactoring regarding the LED-Flashing. - Minimum GainControlRegionOffsetY and GainControlRegionHeight is now 1. - Log mainboard temperature every 5’C temperature change. - More temporary freedom in configuring the MasterSlaveSource/MasterSlaveOutput features. - The validity will be checked before AcquisitionStart or during AcquisitionArm - Checking the LedFlashSequenceTime parameter depends on the LineStart trigger now. - Added NoCache for MasterSlaveSourceReg node for feature update when selecting Default. - Internal refactoring of BPC component **Bug Fixes** - Fixed bugs related to LED-Flashing - Fixed the bug of led flash control in speed2high case - Fixed Bugs regarding loading the Gamma Fixed sensor shut down during over heat. (issue for some hardware) - Fixed the bug in checking line time when led flashing is active. - Fixed the bug in updating the MasterSlaveSource user set entry. (Update from old user set less than 13.0.0) Related to internal line. - Fixed the bug in setting MasterSlaveOutput to off. Fixed bugs related to gain control region. - Fixed the bug for BinningHorizontal when used with ImageCalibrationLineDistance. (Related to DVAL relaxation) - Fixed the bug of artifacts in led flash control - Fixed the bug of led flash control to work with all cxp link configurations Fixed bug when using LED-Flash with only one pattern. - Fixed bug of failing discovery with Matrox/Zebra Grabbers if no region is on. **Incompatibilities** - LED-Flashing - In order to fix LED-Flashing issues the minimum LedFlashSequenceTime has been increased by 0.5us. - This refers also to the minimum value during the triggered mode. - ImageStreamWidthReg feature will not return 0 anymore if no region is enabled, but the sensor width. **Errata** - Using LED-Flash and MasterSlave mode together will not work for the slave camera. - Independently the features are working. - After changing the CxpLinkConfiguration the first line of the first transferred image may be corrupt. | > [!NOTE] > Download Firmware version 13.0.0 > > [Firmware package 13.0.0 allPIXA evo 32k CXP](https://cdn.document360.io/eca58697-9c2f-461e-9f0a-e6205b74b693/Images/Documentation/allPIXAevo_package_p32_cxp_13.0.0.zip) | Camera | Release Notes | | --- | --- | | allPIXA evo 16k CXP | **Changes and New features** - Internal refactoring regarding the LED-Flashing. - Minimum GainControlRegionOffsetY and GainControlRegionHeight is now 1. - Log mainboard temperature every 5’C temperature change. - More temporary freedom in configuring the MasterSlaveSource/MasterSlaveOutput features. - The validity will be checked before AcquisitionStart or during AcquisitionArm - Checking the LedFlashSequenceTime parameter depends on the LineStart trigger now. - Added NoCache for MasterSlaveSourceReg node for feature update when selecting Default. - Internal refactoring of BPC component **Bug Fixes** - Fixed bugs related to LED-Flashing - Fixed the bug of led flash control in speed2high case - Fixed Bugs regarding loading the Gamma Fixed sensor shut down during over heat. (issue for some hardware) - Fixed the bug in checking line time when led flashing is active. - Fixed the bug in updating the MasterSlaveSource user set entry. (Update from old user set less than 13.0.0) Related to internal line. - Fixed the bug in setting MasterSlaveOutput to off. Fixed bugs related to gain control region. - Fixed the bug for BinningHorizontal when used with ImageCalibrationLineDistance. (Related to DVAL relaxation) - Fixed the bug of artifacts in led flash control - Fixed bug of failing discovery with Matrox/Zebra Grabbers if no region is on. **Incompatibilities** - LED-Flashing - In order to fix LED-Flashing issues the minimum LedFlashSequenceTime has been increased by 0.5us. - This refers also to the minimum value during the triggered mode. - ImageStreamWidthReg feature will not return 0 anymore if no region is enabled, but the sensor width. **Errata** - Using LED-Flash and MasterSlave mode together will not work for the slave camera. - Independently the features are working. - LED-Flash - Issues may occur when the sequence period is close to the min sequenece time when using 4 patterns and PixelFormat RGB10 or RGB12 - After changing the CxpLinkConfiguration the first line of the first transferred image may be corrupt. | > [!NOTE] > Download Firmware version 13.0.0 > > [Firmware package 13.0.0 allPIXA evo 16k CXP](https://cdn.document360.io/eca58697-9c2f-461e-9f0a-e6205b74b693/Images/Documentation/allPIXAevo_package_p16_cxp_13.0.0.zip) ### Release 12.0.0 (May 2026) | Camera | New features | | --- | --- | | allPIXA evo 16k CXP | - Introduced support for pixel quality optimization. | | allPIXA evo 32k CXP | > [!NOTE] > Download Firmware version 12.0.0 > > [Firmware package 12.0.0 allPIXA evo 32k CXP](https://cdn.document360.io/eca58697-9c2f-461e-9f0a-e6205b74b693/Images/Documentation/allPIXAevo_package_p32_cxp_12.0.0.zip) > > [Firmware package 12.0.0 allPIXA evo 16k CXP](https://cdn.document360.io/eca58697-9c2f-461e-9f0a-e6205b74b693/Images/Documentation/allPIXAevo_package_p16_cxp_12.0.0.zip) ### Release 10.0.0 (April 2026) | Camera | New features | | --- | --- | | allPIXA evo 16k CXP | - Changed sensor operating mode - Improved image quality - The minimum line time has changed now we support up to ~ 61,6 kHz - Internal refactoring | | allPIXA evo 32k CXP | - Improved reset level control - New sensor configuration requires new DSNU/PRNU reference - Reduced the maximum line rate to ~73KHz - Reduced the ADC-Gain to improve the image quality. - This requires new DSNU/PRNU | > [!NOTE] > Download Firmware version 10.0.0 > > [Release notes allPIXA evo 32k CXP](https://cdn.document360.io/eca58697-9c2f-461e-9f0a-e6205b74b693/Images/Documentation/allPIXA%20evo%2032K%20CXP%20Firmware%20Release%20Notes%2010.0.0.pdf) > > [Firmware package allPIXA evo 32k CXP](https://cdn.document360.io/eca58697-9c2f-461e-9f0a-e6205b74b693/Images/Documentation/allPIXAevo_package_p32_cxp_10.0.0.zip) > > [Release notes allPIXA evo 16k CXP](https://cdn.document360.io/eca58697-9c2f-461e-9f0a-e6205b74b693/Images/Documentation/allPIXA%20evo%2016K%20CXP%20Firmware%20Release%20Notes%2010.0.0.pdf) > > [Firmware package allPIXA evo 16k CXP](https://cdn.document360.io/eca58697-9c2f-461e-9f0a-e6205b74b693/Images/Documentation/allPIXAevo_package_p16_cxp_10.0.0.zip) ### Release 5.0.0 (October 2025) | Camera | New features | | --- | --- | | allPIXA evo 16k CXP allPIXA evo 32k CXP | - Support multi ROI (Region1-4) - Added MultRegionMerge feature to enable single virtual region **RegionStream0** - Allow user set loading even if flat field correction calibration mode is active - Support new feature InfoBlockTriggerSource to trigger the first line info block by an IO - Refactoring on Gain Control (Application supports 12-Ch-BV mono) - The gain control width and offset is limited to certain multiples - If the gain control is outside an ROI the start of the ROI is expected to be precise. - Changed EachLineInfoBlock to the used 8 pixels 2 markers - Adaption of log level of some camera loggings - Added support for new power board 921 - Power file upload can be done outside maintenance mode (if supported) - Extended the power board version string in the DeviceVersion feature - Support Digital IO User Output - Common sensor control (anactrl) for all sensors. - Introduced sensor/acquisition locking (Package must match for camera) | ### Release 3.1.0 (February 2025) | Camera | New features | | --- | --- | | allPIXA evo 16k CXP | - Changed sensor operating mode - Improved image quality - The minimum line time has changed now we support up to ~ 61,6 kHz - Internal refactoring | ### Release 2.9.0 (December 2024) | Camera | New features | | --- | --- | | allPIXA evo 16k CXP | - Added FlashSync line source for evo Line9 - Several improvements in bitstream - Software trigger available for FrameBurstStart - Added two new device status codes for the PX sensor related to reset level - Added new features AcquisitionStatusSelector and AcquisitionStatus | ### Release 2.7.0 (July 2024) | Camera | New features | | --- | --- | | allPIXA evo 16k CXP | Initial Release | ### Release 2.6.0 (July 2024) | Camera | New features | | --- | --- | | allPIXA evo 8k DXGE | Internal refactoring Improvement of the internal voltage control Monitor the g8 training state at runtime | | allPIXA evo 8k CXP | Please refer to the release notes | | allPIXA evo 10K/15K DXGE | Internal refactoring Improvement of the internal voltage control | | allPIXA evo 10K/15K CXP | Please refer to the release notes | ### Release 2.5.0 (April 2024) | Camera | New features | | --- | --- | | allPIXA evo 8k DXGE | Added the DeviceLogLevel feature Support non-volatile logging for better debugging of customer issues The log is accessible by the LogFile in the File Access Control Exposure Time can be changed during grabbing now Changed GevMACAddressConfigReg from MaskedIntReg to IntReg type, to avoid GCT/GenAPI issue Improved order of pixel format initialization during user set load Support FPGA-XADC Added new features for the flat field correction (DSNU/PRNU) | | allPIXA evo 8k CXP | Release skipped | | allPIXA evo 10k DXGE | Added the DeviceLogLevel feature Support non-volatile logging for better debugging of customer issues The log is accessible by the LogFile in the File Access Control Exposure Time can be changed during grabbing now Changed GevMACAddressConfigReg from MaskedIntReg to IntReg type, to avoid GCT/GenAPI issue Improved order of pixel format initialization during user set load Support FPGA-XADC Added new features for the flat field correction (DSNU/PRNU) | | allPIXA evo 10k CXP | Release skipped | | allPIXA evo 15k DXGE | Added the DeviceLogLevel feature Support non-volatile logging for better debugging of customer issues The log is accessible by the LogFile in the File Access Control Exposure Time can be changed during grabbing now Changed GevMACAddressConfigReg from MaskedIntReg to IntReg type, to avoid GCT/GenAPI issue Improved order of pixel format initialization during user set load Support FPGA-XADC Added new features for the flat field correction (DSNU / PRNU) | | allPIXA evo 15k CXP | Release skipped | ### Release 2.4.0 (October 2023) | Camera | New features | | --- | --- | | allPIXA evo 8k DXGE | Support of RGB TDI, Added new Feature to Support different TDI Modes HighSensitivity (new), HighSNR (same as before). Only available for cameras with serial numbers greater than SN: 2278 | | allPIXA evo 8k CXP | Support of RGB TDI, Added new Feature to Support different TDI Modes HighSensitivity (new), HighSNR (same as before). Only available for cameras with serial numbers greater than SN: 2278 | | allPIXA evo 10k DXGE | Release skipped | | allPIXA evo 10k CXP | Release skipped | | allPIXA evo 15k DXGE | Release skipped | | allPIXA evo 15k CXP | Release skipped | ### Release 2.3.0 (July 2023) | Camera | New features | | --- | --- | | allPIXA evo 8k DXGE | IO Analyzer, Optimized black-level control, Support of RGB10, RGB12, Mono10, and Mono12 pixel format | | allPIXA evo 8k CXP | IO Analyzer, Optimized black-level control | | allPIXA evo 10k DXGE | IO Analyzer, Optimized black-level control, Support of RGB10, RGB12, Mono10, and Mono12 pixel format | | allPIXA evo 10k CXP | IO Analyzer, Optimized black-level control | | allPIXA evo 15k DXGE | IO Analyzer, Optimized black-level control, Support of RGB10, RGB12, Mono10, and Mono12 pixel format | | allPIXA evo 15k CXP | IO Analyzer, Optimized black-level control | ### Release 2.2.0 (Mai 2023) | Camera | New features | | --- | --- | | allPIXA evo 8k DXGE | FrameBurstStart | | allPIXA evo 8k CXP | FrameBurstStart Trigger over CXP, LinkTrigger0 and LinkTrigger1 | | allPIXA evo 10k DXGE | Release skipped | | allPIXA evo 10k CXP | Release skipped | | allPIXA evo 15k DXGE | Release skipped | | allPIXA evo 15k CXP | Release skipped | ##