--- title: "Line scan system" slug: "line-scan-system" updated: 2023-07-17T13:44:51Z published: 2023-07-17T13:44:51Z canonical: "docs-linescan.alliedvision.com/line-scan-system" --- > ## Documentation Index > Fetch the complete documentation index at: https://docs-linescan.alliedvision.com/llms.txt > Use this file to discover all available pages before exploring further. # Line scan system | ![svg-line scan system_04](https://cdn.document360.io/eca58697-9c2f-461e-9f0a-e6205b74b693/Images/Documentation/svg-line%20scan%20system_04.svg) | | --- | | **1** | Line scan camera: Scans the image line by line and communicates with the PC. | **2** | Optical system: Lenses and mounts | | **3** | Illumination: Lights up the information carrier/scan area. | **4** | Illumination controller: Controls and monitors the illumination unit. | | **5** | Cables and suitable network card or frame grabber in the PC: The image data are sent to a PC. | **6** | PC: The PC performs subsequent processing of the image data and can optionally control the illumination system. | | **7** | Speed detection: The speed of the object/conveyor belt can be detected by an optional incremental encoder. The encoder can be connected to the camera. | **8** | Conveying unit: Moves the scanned object. | | **9** | Frame trigger: A light barrier can be used to detect the object and start the image acquisition on time. The frame trigger can be connected to the camera. | | |