--- title: "Intended use" slug: "intended-use" updated: 2023-06-23T11:04:21Z published: 2023-06-23T11:04:21Z canonical: "docs-linescan.alliedvision.com/intended-use" --- > ## Documentation Index > Fetch the complete documentation index at: https://docs-linescan.alliedvision.com/llms.txt > Use this file to discover all available pages before exploring further. # Intended use - The device is designed for machines and systems which are used for commercial and industrial applications. - The device is designed for contactless optical detection of primarily two dimensional objects. - The device may only be connected or used as described in this manual. - Do not use the device in safety relevant control circuits and potentially explosive environment.