--- title: "DHCP" slug: "dhcp" updated: 2024-07-04T11:07:12Z published: 2024-07-04T11:07:12Z canonical: "docs-linescan.alliedvision.com/dhcp" --- > ## Documentation Index > Fetch the complete documentation index at: https://docs-linescan.alliedvision.com/llms.txt > Use this file to discover all available pages before exploring further. # DHCP This function is available for firmware release from 5.1 or higher. Set the XLC4 control unit in DHCP mode using command IP D. The DHCP server assigns the XLC4 control unit the IP address. If no DHCP server is available, the programmed standard IP address is used.