--- title: "Control panel Corona II modules" slug: "control-panel-corona-ii-modules" updated: 2025-03-21T10:17:17Z published: 2025-03-21T10:17:17Z canonical: "docs-linescan.alliedvision.com/control-panel-corona-ii-modules" --- > ## Documentation Index > Fetch the complete documentation index at: https://docs-linescan.alliedvision.com/llms.txt > Use this file to discover all available pages before exploring further. # Control panel Corona II modules The control panel is displayed after connecting to a XLC4 control unit. ## Overview control panel ### Informative elements | ![](https://cdn.document360.io/eca58697-9c2f-461e-9f0a-e6205b74b693/Images/Documentation/xlc4commander_control-panel_v01(2).png) | | | --- | --- | | 1 | Current output voltage of LED output channel (X8, X9, X10, X11) | | | 2 | Temperature of the XLC4 control unit and the Corona II module | | | 3 | Serial number of the Corona II module | | | 4 | Number of connected LED boards to the Corona II module | | | 5 | Current input voltage (X4) | | | 6 | Current operating mode | | | 7 | Port name or IP address used by this tab | | | 8 | Selected interface type for connection to the XLC4 control unit | | | 9 | Firmware version of the XLC4 control unit | | | 10 | Serial number of the XLC4 control unit | | ### Functional elements | ![](https://cdn.document360.io/eca58697-9c2f-461e-9f0a-e6205b74b693/Images/Documentation/xlc4commander_control-panel-operating-functions_v01(1).png) | | --- | | 1 | Checkbox *on/off:* Switch Corona II module on or off | | 2 | Input box: Manually enter the LED current value | | 3 | Button *apply:* Activate and store the new value for the LED current | | 4 | Slider: Adjust the LED current value |