--- title: "Connection two cameras with one frame grabber" slug: "connection-two-cameras-with-one-frame-grabber" updated: 2023-01-03T08:56:00Z published: 2023-01-03T08:56:00Z canonical: "docs-linescan.alliedvision.com/connection-two-cameras-with-one-frame-grabber" --- > ## Documentation Index > Fetch the complete documentation index at: https://docs-linescan.alliedvision.com/llms.txt > Use this file to discover all available pages before exploring further. # Connection two cameras with one frame grabber If you want to use two cameras with one frame grabber, you may have to configure the frame grabber (see frame grabber manual). Once it is configured correctly, you can connect the cameras as described in chapter [Connection and disconnection of Camera](/v1/docs/connection-and-disconnection-of-camera)