--- title: "Configure the frame grabber" slug: "configure-the-frame-grabber" updated: 2026-09-02T05:51:29Z published: 2026-09-02T05:51:29Z canonical: "docs-linescan.alliedvision.com/configure-the-frame-grabber" --- > ## Documentation Index > Fetch the complete documentation index at: https://docs-linescan.alliedvision.com/llms.txt > Use this file to discover all available pages before exploring further. # Configure the frame grabber ## Configure an Euresys Coaxlink > [!NOTE] > Use the correct firmware > > In order to operate a Allied Vision CXP camera with an euresys frame grabber, the correct firmware must be loaded on the frame grabber. To check the firmware version and change it if necessary, please follow the steps below: | 1. Open the Euresys Firmware Manager | ![](https://cdn.document360.io/eca58697-9c2f-461e-9f0a-e6205b74b693/Images/Documentation/image-1714384735403.png) | | --- | --- | | 2. Select the frame grabber | | | 3. Chech the firmware version | ![](https://cdn.document360.io/eca58697-9c2f-461e-9f0a-e6205b74b693/Images/Documentation/image-1714389012910.png) it is required to use the following variants: - Variante “1-camera” revision X - Variante “2-camera” revision X - Variante “4-camera” revision X Please do not use the line-scan firmware | | 4. Change the firmware version | ![](https://cdn.document360.io/eca58697-9c2f-461e-9f0a-e6205b74b693/Images/Documentation/image-1714389046807.png) To change the firmware: - Select the correct firmware version - Press “Proceed” and wait until the download is finished - Power-cycle the PC |