--- title: "Configure Channels" slug: "configure-channels" updated: 2024-07-03T15:13:53Z published: 2024-07-04T11:12:48Z canonical: "docs-linescan.alliedvision.com/configure-channels" stale: true --- > ## Documentation Index > Fetch the complete documentation index at: https://docs-linescan.alliedvision.com/llms.txt > Use this file to discover all available pages before exploring further. # Configure Channels During the boot process the XLC4 control unit checks the ports for connected Corona II modules. In automatic mode the detected Corona II modules are displayed as a single module. > [!NOTE] > NOTE > > This selection is stored in the registry and is used at the next of XLC4 commander.