--- title: "Command VR" slug: "command-vr" updated: 2024-07-04T11:07:39Z published: 2024-07-04T11:07:39Z canonical: "docs-linescan.alliedvision.com/command-vr" --- > ## Documentation Index > Fetch the complete documentation index at: https://docs-linescan.alliedvision.com/llms.txt > Use this file to discover all available pages before exploring further. # Command VR Command VR is used to query the current firmware version or release of the XLC4 control unit. ## Structure | Command | Notes | | --- | --- | | CommandID | VR | VR works in all XLC4 operating modes | | Parameter | None | | | Parameter | Value | Description | | None | | The current version and release of the XLC4 firmware is coded in the return value | | Response | | | vr , space , version , “,” , release | | General notes | | | | ## Example VR VR 005 , 010