--- title: "Command TE" slug: "command-te" updated: 2024-07-04T11:07:46Z published: 2024-07-04T11:07:46Z canonical: "docs-linescan.alliedvision.com/command-te" --- > ## Documentation Index > Fetch the complete documentation index at: https://docs-linescan.alliedvision.com/llms.txt > Use this file to discover all available pages before exploring further. # Command TE Command TE is used to query the values of the internal temperature sensors of the XLC4 control unit and the Corona II modules. ## Structure | Command | Notes | | --- | --- | | CommandID | TE | TE works in all XLC4 operating modes | | Parameter | None | | | Parameter | Value | Description | | None | | | | Response | | | te , space , tempPair , “,” , tempPair , “,” , tempPair, “,” , tempPair | | | tempPair = tval , [“-” , tval] | | General notes | | | | The value list in the response message contains the temperature values of the four output channels of the XLC4 (channel A first). If Corona II illumination modules are connected, the internal temperature values of the Coronas are added to the corresponding channel temperature values (separated by -). ## Example TE te 23-22 , 22 , 23-21 , 22 Note that only the first channel of a Corona II module is connected to a temperature sensor. The channels with a temperature pair (“-” separated) are connected to the first channel of a Corona II module. In this example, there are 2 Corona II modules connected: - One to channel A and B - One to channel C The TE command can be used to determine the number of connected Corona II modules.