--- title: "Command RS" slug: "command-rs" updated: 2024-07-04T11:10:06Z published: 2024-07-04T11:10:06Z canonical: "docs-linescan.alliedvision.com/command-rs" --- > ## Documentation Index > Fetch the complete documentation index at: https://docs-linescan.alliedvision.com/llms.txt > Use this file to discover all available pages before exploring further. # Command RS Command RS is used to reset the XLC4 control unit. Changed parameters will be applied after the reset. ## Structure | Command | Notes | | --- | --- | | CommandID | RS | RS works in all XLC4 operating modes | | Parameter | None | | | Parameter | Value | Description | | None | | The current values for channel A are queried | | Response | | | | | General notes | | | Applicable for firmware release from 5.002. | ## Example | Query | Response | Action | | --- | --- | --- | | RS | rs | The XLC4 control unit is reset |