--- title: "Command MP" slug: "command-mp" updated: 2024-07-04T11:08:09Z published: 2024-07-04T11:08:09Z canonical: "docs-linescan.alliedvision.com/command-mp" --- > ## Documentation Index > Fetch the complete documentation index at: https://docs-linescan.alliedvision.com/llms.txt > Use this file to discover all available pages before exploring further. # Command MP Command MP is used to set the read period for the inputs in Analog-controlled mode and in PWM-controlled mode. ## Structure | Command | Notes | | --- | --- | | CommandID | MP | MP is only available in Analog-controlled mode and PWM-controlled mode. | | Parameter | None | | | | New MP value | | | Parameter | Value | Description | | None | | The current value is queried. | | New MP value | Integer value | From “500” to “5000” Default value is “1000” Values are in scans per second | | Response | | | mp , space , new MP value | | General notes | | | | ## Example ### Without parameter | Query | Response | | --- | --- | | MP | mp 1000 | The current read period is 1000 scans per second. ### With New MP value | Query | Action | | --- | --- | | MP 2500 | mp 2500 | The read period is set to 2500 scans per second.