--- title: "Command IY" slug: "command-iy" updated: 2024-07-04T11:07:55Z published: 2024-07-04T11:07:55Z canonical: "docs-linescan.alliedvision.com/command-iy" --- > ## Documentation Index > Fetch the complete documentation index at: https://docs-linescan.alliedvision.com/llms.txt > Use this file to discover all available pages before exploring further. # Command IY Command IY is used to query and set the current of the 4 channels of the XLC4 control unit. ## Structure | Command | Notes | | --- | --- | | CommandID | IY | IY is only available in “Command mode” and “Bulb mode” | | Parameter | None | | | | Channel | | | | Current | | | | Currentlist | | | | Save state | | | | Read option | | | Parameter | Value | Description | | None | | Up to firmware release 4.24: The stored values for all channels are queried. From firmware release 4.25: The current values for all channels are queried. | | Channel | “A” | Channel 1 of the XLC4 control unit | | | “B” | Channel 2 of the XLC4 control unit | | | “C” | Channel 3 of the XLC4 control unit | | | “D” | Channel 4 of the XLC4 control unit | | | “E” | Corona II module connected to channel 1 | | | “F” | Corona II module connected to channel 2 | | | “G” | Corona II module connected to channel 3 | | | “H” | Corona II module connected to channel 4 | | Current | Integer value | Defines the output current rating in mA. The value range is from 200 to 1800. The maximum current value may be limited due to a the LED color of a connected Corona II module: - 1500 mA for red, blue, green - 1800 mA for white, IR - 1400 mA for UV | | Currentlist | | | | Save state | “W” | The current values are stored as new default values. | | Read option | “S” | From firmware release 4.25: The stored values are queried. | | Response | | | iy , space , current , current , current , current | | General notes | | | If the value for the current is higher than the maximum value an error is indicated. If no channel is specified the command is applied to all channels. | ## Example ### Without parameter | Query | Response | | --- | --- | | IY | iy 1000 , 1000 , 1000 , 1000 | Returns the stored/current values. ### With Read option | Query | Response | | --- | --- | | IY S | iy 1000 , 1000 , 1000 , 1000 | Returns the stored/current values. ### With Channel | Query | Action | | --- | --- | | IY A 1000 | Channel A is set to 1000 mA | | IY E 450 | Current is set to 450 mA for Corona II module connected to channel 1 | | IY G 500 | Current is set to 500 mA for Corona II module connected to channel 3 | ### With Current | Query | Action | | --- | --- | | IY 1000,1000,1000,500 | Channel A, B and C are set to 1000 mA. Channel D is set to 500 mA. | | IY 1000,1000,1000,500 W | Channel A, B and C are set to 1000 mA. Channel D is set to 500 mA. All values are set as default. | | IY 300 | All channels are set to 300 mA. | ## Store values as default with save state When the character “W” is set at the end of the command IY the values are stored as default values. | Query | Response | | --- | --- | | IY , space , [channel] , space , current , space , “W” | iy , space , channel , space , current , space , “W” iy , space , current , current , current , current , current , space , “W” | Default values are set: - after switching on the XLC4 control unit - after setting the control unit to Bulb mode and switching on again the control unit.