--- title: "Command ID" slug: "command-id" updated: 2024-07-04T11:08:00Z published: 2024-07-04T11:08:00Z canonical: "docs-linescan.alliedvision.com/command-id" --- > ## Documentation Index > Fetch the complete documentation index at: https://docs-linescan.alliedvision.com/llms.txt > Use this file to discover all available pages before exploring further. # Command ID Command ID is used to change the device ID of the XLC4 control unit. ## Structure | Command | Notes | | --- | --- | | CommandID | ID | ID works in all XLC4 operating modes. | | Parameter | None | | | | New device ID | | | Parameter | Value | Description | | None | | The current value is queried. | | New device ID | Integer value | From “1” to “15” | | Response | | | id , space , new device ID | | General notes | | | The ID is coded as decimal values. For addressing, the ID is coded in a single hexadecimal character. The new ID is applied after switching on again. | ## Example ### Without parameter | Query | Response | | --- | --- | | ID | id 11 | Returns the current ID of the XLC4 control unit. ### Without new device ID | Query | Response | | --- | --- | | ID 11 | id 11 | Sets a new ID for the XLC4 control unit.