--- title: "Command ER" slug: "command-er" updated: 2024-07-04T11:10:10Z published: 2024-07-04T11:10:10Z canonical: "docs-linescan.alliedvision.com/command-er" --- > ## Documentation Index > Fetch the complete documentation index at: https://docs-linescan.alliedvision.com/llms.txt > Use this file to discover all available pages before exploring further. # Command ER Command ER is used to query the error state of the XLC4 control unit. ## Structure | Command | Notes | | --- | --- | | CommandID | ER | ER works in all XLC4 operating modes | | Parameter | None | | | reset | | | Parameter | Value | Description | | None | | The error state is queried | | reset | “0” | The error state is reset | | Response | | | er , space , err_state | | General notes | | | You can only reset the error state when the error cause is solved. For more information about the error codes refer to [Error codes](/v1/docs/error-codes). | ## Example | Query | Response | Action | | --- | --- | --- | | ER | er 205 | The error 205 is set | | ER 0 | er 0 | The error state is reset | | ER | er 0 | There are no errors set |