--- title: "Bulb mode" slug: "bulb-mode" updated: 2024-07-04T11:10:20Z published: 2024-07-04T11:10:20Z canonical: "docs-linescan.alliedvision.com/bulb-mode" --- > ## Documentation Index > Fetch the complete documentation index at: https://docs-linescan.alliedvision.com/llms.txt > Use this file to discover all available pages before exploring further. # Bulb mode In the Bulb mode the XLC4 control unit behaves like a classical bulb lamp. When the power supply in on the LEDs are switched on. Use the bulb mode for a certain amount of lighting, for example switching the LEDs on once per day. Do not use it for flashing applications. | Parameter | Value | | --- | --- | | cuPar.WorkingMode | 0 | The XLC4 control unit provides constant output currents for all 4 output channels. The amount of output currents is preset by a command and stored permanently in the registers cuPar.DefaultCurrent[0…3]. Change the content of the registers with the command IY: - IY , [channel] , current , “W” | - IY , current , current , current , current , “W